This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ti SDK 6.0.0

Hello,

I am using BeagleboardXm along with the TiSDK 6.0.0 

I have loaded the image in SD card and my matrix app launcher is running correctly. 

My question is after booting I dont know what to do for 

/**************************/

beagleboard login : 

/**************************/

what will be the login  after that it is asking for password what should i do ? 

2nd question is can we run the qt4 application through this Ti-SDK  ? and remote debugging  ? 

Please forgive the mistakes considering as newbie 

Thank you,

nilesh

  • Hi Nilesh,

    The login name with the TI-SDK is usually "root" with no password needed.

    Regarding your QT question I can only provide some useful wiki pages:

    Building QT
    QT projects in CCS5
    Sitara Linux Training: Hands on with QT

    Best regards,
    Miroslav

  • Hi Miroslav thanx for quick reply, 

    after booting I am getting th following msg

    Starting Matrix GUI application.
    ***************************************************************
    ***************************************************************
    NOTICE: This file system contains the followin GPLv3 packages:
    binutils-symlinks
    binutils
    gdbserver

    If you do not wish to distribute GPLv3 components please remove
    the above packages prior to distribution. This can be done using
    the opkg remove command. i.e.:
    opkg remove <package>
    Where <package> is the name printed in the list above

    NOTE: If the package is a dependency of another package you
    will be notified of the dependent packages. You should
    use the --force-removal-of-dependent-packages option to
    also remove the dependent packages as well
    ***************************************************************
    ***************************************************************

    do I have to install above mentioned packages?

    because "beabale login : root " is also asking for password 

    OR do i have to start again ? 

  • Hi,

    These messages have nothing to do with your issue. They have to do with package licensing information.

    Using the TI SDK rootfs, the "root" user should have no password. Please check the /etc/passwd file in the SDK rootfs on your SD card for this line (should be the first):

    root:x:0:0:root:/home/root:/bin/sh

    You probably have this "x" I have marked in red. Remove it, save the file and try again with the SD card. The first line should look like this:

    root::0:0:root:/home/root:/bin/sh

    If it still doesn't work, then please post the contents of the /etc/shadow file from your SDK rootfs.

    Best regards,
    Miroslav

  • Hello Morislav ,

    thank you for your link I have just followed that link instruction and I hv got the problem.

    Thank you for support,

    Nilesh

  • Hi, Miroslav 

    I have changed the etc/passwd file as you have suggested it is working perfectly.

    root::0:0:root:/home/root:/bin/sh

    Thank you so much 

    Nilesh