This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

exception comes after switch from lowpower to fullfeature mode

Hi ,Ti experts:

DM8127 IPNC RDK 3.5.

for some reason,when i switch from lowpower to fullfeature mode,some exception comes.

boot log as follow attachment.


U-Boot 2010.06 (Aug 15 2013 - 10:52:49) DM8127_IPNC_3.50.00

TI8148-GP rev 2.1

ARM clk: 600MHz
DDR clk: 400MHz
L3 clk: 200MHz
IVA clk: 450MHz
ISS clk: 400MHz
DSP Default OFF
DSS Default OFF

DRAM:  512 MiB
NAND:  HW ECC BCH8 Selected
256 MiB
Using default environment

The 2nd stage U-Boot will now be auto-loaded
Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is already flashed
Hit any key to stop autoboot:  0 

NAND read: device 0 offset 0x20000, size 0x40000
 262144 bytes read: OK
## Starting application at 0x81000000 ...


U-Boot 2010.06 (Aug 15 2013 - 10:54:21) DM8127_IPNC_3.50.00

TI8148-GP rev 2.1

ARM clk: 600MHz
DDR clk: 400MHz
L3 clk: 200MHz
IVA clk: 450MHz
ISS clk: 400MHz
DSP Default OFF
DSS Default OFF

I2C:   ready
DRAM:  512 MiB
NAND:  HW ECC BCH8 Selected
256 MiB
MMC:   OMAP SD/MMC: 0, ON-BOARD SDIO: 1
                          .:;rrr;;.                   
                    ,5#@@@@#####@@@@@@#2,             
                 ,A@@@hi;;;r5;;;;r;rrSG@@@A,          
               r@@#i;:;s222hG;rrsrrrrrr;ri#@@r        
             :@@hr:r;SG3ssrr2r;rrsrsrsrsrr;rh@@:      
            B@H;;rr;3Hs;rrr;sr;;rrsrsrsrsrsr;;H@B     
           @@s:rrs;5#;;rrrr;r#@H:;;rrsrsrsrsrr:s@@    
          @@;;srs&X#9;r;r;;,2@@@rrr:;;rrsrsrsrr;;@@   
         @@;;rrsrrs@MB#@@@@@###@@@@@@#rsrsrsrsrr;;@@  
        G@r;rrsrsr;#X;SX25Ss#@@#M@#9H9rrsrsrsrsrs;r@G 
        @9:srsrsrs;2@;:;;:.X@@@@@H::;rrsrsrsrsrsrr:3@ 
       X@;rrsrsrsrr;XAi;;:&@@#@Bs:rrsrsrsrsrsrsrsrr;@X
       @#;rsrsrsrsrr;r2ir@@@###::rrsrsrsrsrsrsrsrsr:@@
       @A:rrsrsrsrr;:2@29@@M@@@;:;rrrrsrsrsrsrsrsrs;H@
       @&;rsrsrsrr;A@@@@@@###@@@s::;:;;rrsrsrsrsrsr;G@
       @#:rrsrsrsr;G@5Hr25@@@#@@@#9XG9s:rrrrsrsrsrs:#@
       M@;rsrsrsrs;r@&#;::S@@@@@@@M@@@@Grr:;rsrsrsr;@#
       :@s;rsrsrsrr:M#Msrr;;&#@@@@@@@@@@H@@5;rsrsr;s@,
        @@:rrsrsrsr;S@rrrsr;:;r3MH@@#@M5,S@@irrsrr:@@ 
         @A:rrsrsrsrrrrrsrsrrr;::;@##@r:;rH@h;srr:H@  
         ;@9:rrsrsrsrrrsrsrsrsr;,S@Hi@i:;s;MX;rr:h@;  
          r@B:rrrrsrsrsrsrsrr;;sA@#i,i@h;r;S5;r:H@r   
           ,@@r;rrrsrsrsrsrr;2BM3r:;r:G@:rrr;;r@@,    
             B@Mr;rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H      
              .@@@i;;rrrrsrs2i;rrrrr;r@M:;i@@@.       
                .A@@#5r;;;r;;;rrr;r:r#AsM@@H.         
                   ;&@@@@MhXS5i5SX9B@@@@G;            
                       :ihM#@@@@@##hs,                

Date: 2012-11-09 (Friday)    Time: 14:30:48
Net:   Detected MACID:84:7e:40:e:eb:80
cpsw
Hit any key to stop autoboot:  2  1  0 
link up on port 0, speed 1000, full duplex
Using cpsw device
TFTP from server 192.168.1.120; our IP address is 192.168.1.143
Filename 'uImage'.
Load address: 0x81000000
Loading: *#################################################################
	 #################################################################
	 #################################################################
	 #################################################################
	 #################################################################
	 #################################################################
	 #################################################################
	 ################################
done
Bytes transferred = 2493092 (260aa4 hex)
## Booting kernel from Legacy Image at 81000000 ...
   Image Name:   Linux-2.6.37_DM8127_IPNC_3.50.00
   Created:      2013-08-15  15:07:24 UTC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2493028 Bytes = 2.4 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37_DM8127_IPNC_3.50.00 (root@localhost.localdomain) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Thu Aug 15 11:07:15 EDT 2013

CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: ti8148ipnc

vram size = 4194304 at 0x0

bootconsole [earlycon0] enabled

ti81xx_reserve: ### Reserved DDR region @84f00000

reserved size = 4194304 at 0x0

FB: Reserving 4194304 bytes SDRAM for VRAM

Memory policy: ECC disabled, Data cache writeback

OMAP chip is TI8148 2.1

SRAM: Mapped pa 0x402f1000 to va 0xfe400000 size: 0xf000

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 19040

Kernel command line: console=ttyO0,115200n8 root=/dev/nfs rw mem=80M vram=4M notifyk.vpssm3_sva=0xBFD00000 rootdelay=3 nfsroot=192.168.1.120:/home/simon/test/dm8127_ipnc/Source/ipnc_rdk/target/filesys,nolock eth=84:7e:40:0e:eb:80 ip=192.168.1.143 cmemk.phys_start=0x85000000 cmemk.phys_end=0x89000000 cmemk.allowOverlap=1 earlyprintk

cpsw: kernel boot params Ethernet address: 84:7e:40:0e:eb:80

PID hash table entries: 512 (order: -1, 2048 bytes)

Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)

Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)

Memory: 74MB 1MB = 75MB total

Memory: 70652k/70652k available, 11268k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xffc00000 - 0xffe00000   (   2 MB)

    vmalloc : 0xc5800000 - 0xf8000000   ( 808 MB)

    lowmem  : 0xc0000000 - 0xc5000000   (  80 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .init : 0xc0008000 - 0xc003e000   ( 216 kB)

      .text : 0xc003e000 - 0xc04bf000   (4612 kB)

      .data : 0xc04c0000 - 0xc05004c0   ( 258 kB)

SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

NR_IRQS:375

IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts

Total of 128 interrupts on 1 active controller

GPMC revision 6.0

Trying to install interrupt handler for IRQ368

Trying to install interrupt handler for IRQ369

Trying to install interrupt handler for IRQ370

Trying to install interrupt handler for IRQ371

Trying to install interrupt handler for IRQ372

Trying to install interrupt handler for IRQ373

Trying to install interrupt handler for IRQ374

Trying to install type control for IRQ375

Trying to set irq flags for IRQ375

OMAP clockevent source: GPTIMER1 at 20000000 Hz

Console: colour dummy device 80x30

Calibrating delay loop... 599.65 BogoMIPS (lpj=2998272)

pid_max: default: 32768 minimum: 301

Security Framework initialized

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

devtmpfs: initialized

TI81XX: Map 0x84f00000 to 0xfe500000 for dram barrier

TI81XX: Map 0x40300000 to 0xfe600000 for sram barrier

omap_voltage_early_init: voltage driver support not added

regulator: core version 0.5

regulator: dummy: 

NET: Registered protocol family 16

omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!

omap_voltage_add_dev: VDD specified does not exist!

OMAP GPIO hardware version 0.1

OMAP GPIO hardware version 0.1

OMAP GPIO hardware version 0.1

OMAP GPIO hardware version 0.1

omap_mux_init: Add partition: #1: core, flags: 4

_omap_mux_init_gpio: Could not set gpio79

_omap_mux_init_gpio: Could not set gpio80

Cannot clk_get ck_32

Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now

registered ti81xx_vpss device

registered ti81xx_vidout device

registered ti81xx on-chip HDMI device

registered ti81xx_fb device

PWM0 init success.

PWM1 init success.

bio: create slab <bio-0> at 0

SCSI subsystem initialized

USBSS revision 4ea2080b

registerd cppi-dma Intr @ IRQ 17

Cppi41 Init Done

omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz

regulator: VRTC: 1800 mV 

regulator: VIO: 1500 mV 

regulator: VDD1: 600 <--> 1500 mV at 1100 mV 

regulator: VDD2: 600 <--> 1500 mV at 1350 mV 

regulator: VDDCTRL: 600 <--> 1400 mV at 1200 mV 

regulator: LDO1: 1100 <--> 3300 mV at 1800 mV 

regulator: LDO2: 1100 <--> 3300 mV at 1800 mV 

regulator: LDO3: 1100 <--> 3300 mV at 3300 mV 

regulator: LDO4: 1100 <--> 3300 mV at 1800 mV 

regulator: LDO5: 1100 <--> 3300 mV at 3300 mV 

regulator: LDO6: 1100 <--> 3300 mV at 3300 mV 

regulator: LDO7: 1100 <--> 3300 mV at 3300 mV 

regulator: LDO8: 1100 <--> 3300 mV at 1800 mV 

tps65911-rtc tps65911-rtc: rtc core: registered tps65911-rtc as rtc0

tps65910 1-002d: No interrupt support, no core IRQ

Advanced Linux Sound Architecture Driver Version 1.0.23.

Switching to clocksource gp timer

musb-hdrc: version 6.0, peripheral, debug=0

musb-hdrc musb-hdrc.0: dma type: dma-cppi41

MUSB controller-0 revision 4ea20800

usb2phy: computed values rxcalib(15)DACs(30 14 13)

usb2phy: override computed values rxcalib(15)DACs(30 14 13)

usb2phy_config: musb(0) rxcalib done, rxcalib read value 6f6f5d6e

musb-hdrc musb-hdrc.0: USB Peripheral mode controller at c581e000 using DMA, IRQ 18

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 4096 (order: 3, 32768 bytes)

TCP bind hash table entries: 4096 (order: 2, 16384 bytes)

TCP: Hash tables configured (established 4096 bind 4096)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

NetWinder Floating Point Emulator V0.97 (double precision)

PMU: registered new PMU device of type 0

omap-iommu omap-iommu.0: ducati registered

omap-iommu omap-iommu.1: sys registered

JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

msgmni has been set to 137

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

CMEMK module: built on Aug 15 2013 at 10:56:26

  Reference Linux version 2.6.37

  File /home/simon/test/dm8127_ipnc/Source/ti_tools/linuxutils_3_23_00_01/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c

allocated heap buffer 0xc7000000 of size 0x4000000

cmemk initialized

Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled

omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0

console [ttyO0] enabled, bootconsole disabled
console [ttyO0] enabled, bootconsole disabled

omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
brd: module loaded
loop: module loaded
omap2-nand driver initializing
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron )
Creating 8 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x000006fc0000 : "File System"
0x000006fc0000-0x000007bc0000 : "Data"
0x000007bc0000-0x00000b0c0000 : "File System2"
0x00000b0c0000-0x000010000000 : "Reserved"
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffffe
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
mice: PS/2 mouse device common for all mice
i2c /dev entries driver
Linux video capture interface: v2.00
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
notify_init : notify drivercreated  for  remote proc id 2 at physical Address 0xbfd00000
cm: Module associated with clock hdmi_i2s_fck didn't enable in 100000 tries
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
asoc: HDMI-DAI-CODEC <-> hdmi-dai mapping ok
ALSA device list:
  #0: TI8148 IPNC
nf_conntrack version 0.5.0 (1103 buckets, 4412 max)
ip_tables: (C) 2000-2006 Netfilter Core Team
TCP cubic registered
NET: Registered protocol family 17
Bridge firewalling registered
lib80211: common routines for IEEE802.11 drivers
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
Detected MACID=84:7e:40:e:eb:80
tps65911-rtc tps65911-rtc: setting system clock to 2012-11-09 14:31:01 UTC (1352471461)

CPSW phy found : id is : 0x4dd074
PHY 0:01 not found
IP-Config: Guessing netmask 255.255.255.0
IP-Config: Complete:
     device=eth0, addr=192.168.1.143, mask=255.255.255.0, gw=255.255.255.255,
     host=192.168.1.143, domain=, nis-domain=(none),
     bootserver=255.255.255.255, rootserver=192.168.1.120, rootpath=
Waiting 3sec before mounting root device...
PHY: 0:00 - Link is Up - 1000/Full
VFS: Mounted root (nfs filesystem) on device 0:14.
devtmpfs: mounted
Freeing init memory: 216K

INIT: version 2.86 booting

Please wait: booting...
Starting udev
Root filesystem already rw, not remounting
Caching udev devnodes
root: mount: mounting /dev/root on / failed: No such file or directory
NOT configuring network interfaces: / is an NFS mount
rm: cannot remove '/tmp': Device or resource busy
 inside finish.sh 
UBI: attaching mtd5 to ubi0
UBI: physical eraseblock size:   131072 bytes (128 KiB)
UBI: logical eraseblock size:    126976 bytes
UBI: smallest flash I/O unit:    2048
UBI: sub-page size:              512
UBI: VID header offset:          2048 (aligned 2048)
UBI: data offset:                4096
UBI: max. sequence number:       56
UBI: attached mtd5 to ubi0
UBI: MTD device name:            "Data"
UBI: MTD device size:            12 MiB
UBI: number of good PEBs:        96
UBI: number of bad PEBs:         0
UBI: number of corrupted PEBs:   0
UBI: max. allowed volumes:       128
UBI: wear-leveling threshold:    4096
UBI: number of internal volumes: 1
UBI: number of user volumes:     1
UBI: available PEBs:             0
UBI: total number of reserved PEBs: 96
UBI: number of PEBs reserved for bad PEB handling: 2
UBI: max/mean erase counter: 3/1
UBI: image sequence number:  -161027269
UBI: background thread "ubi_bgt0d" started, PID 255
UBI device number 0, total 96 LEBs (12189696 bytes, 11.6 MiB), available 0 LEBs (0 bytes), LEB size 126976 bytes (124.0 KiB)
UBIFS: recovery needed
UBIFS: recovery completed
UBIFS: mounted UBI device 0, volume 0, name "ubifs_volume"
UBIFS: file system size:   10285056 bytes (10044 KiB, 9 MiB, 81 LEBs)
UBIFS: journal size:       1015809 bytes (992 KiB, 0 MiB, 6 LEBs)
UBIFS: media format:       w4/r0 (latest is w4/r0)
UBIFS: default compressor: lzo
UBIFS: reserved for root:  485787 bytes (474 KiB)
UBI: attaching mtd7 to ubi1
UBI: physical eraseblock size:   131072 bytes (128 KiB)
UBI: logical eraseblock size:    126976 bytes
UBI: smallest flash I/O unit:    2048
UBI: sub-page size:              512
UBI: VID header offset:          2048 (aligned 2048)
UBI: data offset:                4096
UBI: max. sequence number:       582
UBI: attached mtd7 to ubi1
UBI: MTD device name:            "Reserved"
UBI: MTD device size:            79 MiB
UBI: number of good PEBs:        634
UBI: number of bad PEBs:         0
UBI: number of corrupted PEBs:   0
UBI: max. allowed volumes:       128
UBI: wear-leveling threshold:    4096
UBI: number of internal volumes: 1
UBI: number of user volumes:     1
UBI: available PEBs:             0
UBI: total number of reserved PEBs: 634
UBI: number of PEBs reserved for bad PEB handling: 6
UBI: max/mean erase counter: 31/30
UBI: image sequence number:  954328092
UBI: background thread "ubi_bgt1d" started, PID 267
UBI device number 1, total 634 LEBs (80502784 bytes, 76.8 MiB), available 0 LEBs (0 bytes), LEB size 126976 bytes (124.0 KiB)
UBIFS: recovery needed
UBIFS: recovery completed
UBIFS: mounted UBI device 1, volume 0, name "ubifs_volume"
UBIFS: file system size:   78090240 bytes (76260 KiB, 74 MiB, 615 LEBs)
UBIFS: journal size:       3936256 bytes (3844 KiB, 3 MiB, 31 LEBs)
UBIFS: media format:       w4/r0 (latest is w4/r0)
UBIFS: default compressor: lzo
UBIFS: reserved for root:  3688395 bytes (3601 KiB)
./init.sh: line 5: -f: not found
numid=1,iface=MIXER,name='PCM Playback Volume'
  ; type=INTEGER,access=rw---R--,values=2,min=0,max=127,step=0
  : values=127,127
  | dBscale-min=-63.50dB,step=0.50dB,mute=0
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
SysLink version : 2.20.02.20
SysLink module created on Date:Aug 15 2013 Time:11:09:09
Trace enabled
Trace SetFailureReason enabled
/dev/mem opened.
             Phy Addr : 0x48181560 Data : 0x00000002
secss put in low power state
             Phy Addr : 0x48180f10 Data : 0x00000000
             Phy Addr : 0x48180508 Data : 0x00000302
             Phy Addr : 0x48180520 Data : 0x00000002
             Phy Addr : 0x48180524 Data : 0x00000002
             Phy Addr : 0x48180528 Data : 0x00000002
             Phy Addr : 0x4c0000e4 Data : 0x00170208
             Phy Addr : 0x4d0000e4 Data : 0x00170208
             Phy Addr : 0x4c0000e4 Data : 0x00170208
             Phy Addr : 0x4d0000e4 Data : 0x00170208
DDR IOs RX is shutdown 


 [host]  Setting L3 bandwidth regulator for [HDVICP0 ] to [press=[0,0] BW=900, WM Cycles=2500]
Creat queue id:0
queue id:0
FileMngThread created
Creat queue id:32769
queue id:32769
AlramThread created
Share memory init success


 [host]  Setting DMM priority for [ISS     ] to [0] ( 0x4e000634 = 0x00800000 )
Creat queue id:65538
queue id:65538
Creat queue id:98307
queue id:98307
queue id:32769


 [host]  Setting DMM priority for [HDVICP0 ] to [1] ( 0x4e000634 = 0x00000009 )
IPNC_3.50.00 (root@localhost.localdomain) (gcc version 4.5.3 20110311 ( 


 [host] Attached to slave procId 2.


 [host] Attached to slave procId 1.


 [host] Loaded file ./firmware/ipnc_rdk_fw_m3vpss.xem3 on slave procId 2.
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040


 [host] Started slave procId 2.


 [host] After Ipc_loadcallback status [0x00000000]


 [host] Attached to slave procId 0.


 [host] Loaded file ./firmware/ipnc_rdk_fw_m3video.xem3 on slave procId 1.
 [m3vpss ] ***** SYSTEM  : Frequency <ORG> - 200000000, <NEW> - 200000000
 [m3vpss ] notify_attach  rtnVal  0
 [m3vpss ] initProxyServer  rtnVal  0
 [m3vpss ]  
 [m3vpss ]  *** UTILS: CPU KHz = 400000 Khz ***
 [m3vpss ]  
 [m3vpss ]  91: SYSTEM  : System Common Init in progress !!!
 [m3vpss ]  91: SYSTEM: IPC init in progress !!!
 [m3vpss ]  91: SYSTEM: Attaching to [HOST] ... 


 [host] Started slave procId 1.


 [host] After Ipc_loadcallback status [0x00000000]
 [m3video] ***** SYSTEM  : Frequency <ORG> - 200000000, <NEW> - 200000000
 [m3video]  
 [m3video]  *** UTILS: CPU KHz = 400000 Khz ***
 [m3video]  
 [m3video]  141: SYSTEM  : System Common Init in progress !!!
 [m3video]  141: SYSTEM: IPC init in progress !!!
 [m3video]  142: SYSTEM: Attaching to [HOST] ... 


 [host] Loaded file ./firmware/ipnc_rdk_fw_c6xdsp.xe674 on slave procId 0.


 [host] Started slave procId 0.


 [host] After Ipc_loadcallback status [0x00000000]
 [c6xdsp ] ***** SYSTEM  : Frequency <ORG> - 500000000, <NEW> - 500000000
 [c6xdsp ]  
 [c6xdsp ]  *** UTILS: CPU KHz = 500000 Khz ***
 [c6xdsp ]  
 [c6xdsp ]  1: SYSTEM  : System Common Init in progress !!!
 [c6xdsp ]  1: SYSTEM: IPC init in progress !!!
 [c6xdsp ]  1: SYSTEM: Attaching to [HOST] ... 


 [host] After Ipc_startcallback status [0x00000000]
 [m3video]  1141: SYSTEM: Attaching to [HOST] ... 
 [m3vpss ]  1091: SYSTEM: Attaching to [HOST] ... 
 [m3vpss ]  1094: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
 [m3vpss ]  1094: SYSTEM: Attaching to [DSP] ... 
 [m3video]  1150: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
 [m3video]  1150: SYSTEM: Attaching to [DSP] ... 


 [host] After Ipc_startcallback status [0x00000000]
 [c6xdsp ]  1001: SYSTEM: Attaching to [HOST] ... 
 [c6xdsp ]  1004: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
 [c6xdsp ]  1004: SYSTEM: Attaching to [VIDEO-M3] ... 


 [host] After Ipc_startcallback status [0x00000000]
 [m3vpss ]  2094: SYSTEM: Attaching to [DSP] ... 
 [m3video]  2149: SYSTEM: Attaching to [DSP] ... 
 [c6xdsp ]  2003: SYSTEM: Attaching to [VIDEO-M3] ... 
 [m3vpss ]  3094: SYSTEM: Attaching to [DSP] ... 
 [c6xdsp ]  2953: SYSTEM: Attaching to [VIDEO-M3] ... SUCCESS !!!
 [m3video]  3149: SYSTEM: Attaching to [DSP] ... 
 [c6xdsp ]  2953: SYSTEM: Attaching to [VPSS-M3] ... 
 [m3video]  3150: SYSTEM: Attaching to [DSP] ... SUCCESS !!!
 [m3video]  3150: SYSTEM: Attaching to [VPSS-M3] ... 
 [m3vpss ]  4094: SYSTEM: Attaching to [DSP] ... 
 [c6xdsp ]  3952: SYSTEM: Attaching to [VPSS-M3] ... 
 [m3video]  4149: SYSTEM: Attaching to [VPSS-M3] ... 
 [c6xdsp ]  4897: SYSTEM: Attaching to [VPSS-M3] ... SUCCESS !!!
 [m3vpss ]  5094: SYSTEM: Attaching to [DSP] ... 
 [c6xdsp ]  4898: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
 [m3vpss ]  5094: SYSTEM: Attaching to [DSP] ... SUCCESS !!!
 [m3vpss ]  5095: SYSTEM: Attaching to [VIDEO-M3] ... 
 [m3video]  5149: SYSTEM: Attaching to [VPSS-M3] ... 
 inside autorun 

INIT: Entering runlevel: 5

 sbulla: unknown partition table
 [c6xdsp ]  5897: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
 [m3video]  6095: SYSTEM: Attaching to [VPSS-M3] ... SUCCESS !!!
 [m3vpss ]  6094: SYSTEM: Attaching to [VIDEO-M3] ... 
 [m3video]  6095: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
 [m3vpss ]  6095: SYSTEM: Attaching to [VIDEO-M3] ... SUCCESS !!!
 [m3video]  6095: SYSTEM: Creating MsgQ [VIDEO-M3_MSGQ] ...
 [m3vpss ]  6095: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
 [m3video]  6096: SYSTEM: Creating MsgQ [VIDEO-M3_ACK_MSGQ] ...
 [m3vpss ]  6095: SYSTEM: Creating MsgQ [VPSS-M3_MSGQ] ...
 [m3video]  6098: SYSTEM: Notify register to [HOST] line 0, event 12 ... 
 [m3vpss ]  6095: SYSTEM: Creating MsgQ [VPSS-M3_ACK_MSGQ] ...
 [m3video]  6098: SYSTEM: Notify register to [DSP] line 0, event 12 ... 
 [m3vpss ]  6098: SYSTEM: Notify register to [HOST] line 0, event 12 ... 
 [m3video]  6098: SYSTEM: Notify register to [VPSS-M3] line 0, event 12 ... 
 [m3vpss ]  6098: SYSTEM: Notify register to [DSP] line 0, event 12 ... 
 [m3video]  6098: SYSTEM: IPC init DONE !!!
 [m3vpss ]  6098: SYSTEM: Notify register to [VIDEO-M3] line 0, event 12 ... 
 [m3vpss ]  6098: SYSTEM: IPC init DONE !!!
 [m3vpss ] Received character 's'
 [m3video]  6108: MEM: Shared Region 2: Base = 0xb8000000, Length = 0x06900000 (105 MB) 
 [m3vpss ]  6108: MEM: Shared Region 2: Base = 0xb8000000, Length = 0x06900000 (105 MB) 
 [m3video]  6109: MEM: Shared Region 1: Base = 0x89000000, Length = 0x03c00000 (60 MB) 
 [m3vpss ]  6108: MEM: Shared Region 1: Base = 0x89000000, Length = 0x03c00000 (60 MB) 
 [m3video]  6111: SYSTEM  : System Common Init Done !!!
 [m3vpss ]  6111: SYSTEM  : System Common Init Done !!!
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff000 sbulla: unknown partition table
00
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
 [m3video] Received character 's'
Starting telnet daemon [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
.
Starting syslogd/klogd: done
c
 _____                    _____           _         _   
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
              |___|                    |___|            

Arago Project http://arago-project.org dm814x-evm ttyO0

Arago 2011.09 dm814x-evm ttyO0

dm814x-evm login: root (automatic login)
root@dm814x-evm:~#  [c6xdsp ]  6897: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
 [c6xdsp ]  6897: SYSTEM: Creating MsgQ [DSP_MSGQ] ...
 [c6xdsp ]  6898: SYSTEM: Creating MsgQ [DSP_ACK_MSGQ] ...
 [c6xdsp ]  6898: SYSTEM: Notify register to [HOST] line 0, event 12 ... 
 [c6xdsp ]  6898: SYSTEM: Notify register to [VIDEO-M3] line 0, event 12 ... 
 [c6xdsp ]  6898: SYSTEM: Notify register to [VPSS-M3] line 0, event 12 ... 
 [c6xdsp ]  6899: SYSTEM: IPC init DONE !!!
 [c6xdsp ] Received character 's'
 [c6xdsp ]  6902: MEM: Shared Region 2: Base = 0xb8000000, Length = 0x06900000 (105 MB) 
 [c6xdsp ]  6902: MEM: Shared Region 1: Base = 0x89000000, Length = 0x03c00000 (60 MB) 
 [c6xdsp ]  6903: SYSTEM  : System Common Init Done !!!
queue id:65538

CPU is TI812x
Error: SemWait: Invalid Semaphore handler
Error: SemRelease: Invalid Semaphore handler

*****************************************************************

    IPNC BUILD VERSION: DM8127 IPNC RDK VERSION 03.50.00.08	

*****************************************************************

./bin/ipnc_rdk_mcfw.out   VNF_QUALITY TRISTREAM TRIPLE_H264 TI2A AEWB 1080P_D1 H264 HIGH_SPEED1 H264 HIGH_SPEED2 MJPEG 80 &
Error: SemWait: Invalid Semaphore handler
Error: SemRelease: Invalid Semaphore handler
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
 [m3vpss ]  7311: SYSTEM  : System VPSS Init in progress !!!
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
 [m3vpss ] === I2C0/2 Clk is active ===
 [m3vpss ]  7329: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_0] in region 0 ...
 [m3vpss ]  7330: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_0] in region 0 ...
 [m3vpss ]  7330: SYSTEM: ListElem Shared Addr = 0xbe98b680
 [m3vpss ]  7333: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_1] in region 0 ...
 [m3vpss ]  7333: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_1] in region 0 ...
 [m3vpss ]  7333: SYSTEM: ListElem Shared Addr = 0xbe98eb80
 [m3vpss ]  7348: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_23] in region 0 ...
 [m3vpss ]  7348: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_23] in region 0 ...
 [m3vpss ]  7348: SYSTEM: ListElem Shared Addr = 0xbe992080
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
 [m3vpss ]  7351: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_24] in region 0 ...
 [m3vpss ]  7351: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_24] in region 0 ...
 [m3vpss ]  7352: SYSTEM: ListElem Shared Addr = 0xbe9b1a80
 [m3vpss ]  7354: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_25] in region 0 ...
 [m3vpss ]  7355: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_25] in region 0 ...
 [m3vpss ]  7355: SYSTEM: ListElem Shared Addr = 0xbe9d1480
 [m3vpss ]  7362: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_28] in region 0 ...
 [m3vpss ]  7362: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_28] in region 0 ...
 [m3vpss ]  7363: SYSTEM: ListElem Shared Addr = 0xbe9f0e80
 [m3vpss ]  7365: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_29] in region 0 ...
 [m3vpss ]  7366: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_29] in region 0 ...
 [m3vpss ]  7366: SYSTEM: ListElem Shared Addr = 0xbea0ab00
 [m3vpss ]  7368: SYSTEM : HDVPSS Drivers Version: HDVPSS_01_00_01_37
 [m3vpss ]  7368: SYSTEM  : FVID2 Init in progress !!!
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
mkdosfs 3.0.12 (29 Oct 2011)
 [c6xdsp ]  7201: SYSTEM  : System DSP Init in progress !!!
unable to get drive geometry, using default 255/63
/dev/sbulla has 255 heads and 63 sectors per track,
logical sector size is 512,
using 0xf8 media descriptor, with 1024 sectors;
file system has 2 12-bit FATs and 4 sectors per cluster.
FAT size is 1 sector, and provides 247 clusters.
There is 1 reserved sector.
Root directory contains 512 slots and uses 32 sectors.
Volume ID is 33a3b28e, no volume label.
 [c6xdsp ]  7207: SYSTEM: Creating ListMP [DSP_IPC_OUT_23] in region 0 ...
 [c6xdsp ]  7207: SYSTEM: Creating ListMP [DSP_IPC_IN_23] in region 0 ...
 [c6xdsp ]  7207: SYSTEM: ListElem Shared Addr = 0xbea24780
 [c6xdsp ]  7208: SYSTEM: Creating Lg_file_storage gadget: No serial-number string provided!
istMP [DSP_IPC_Og_file_storage gadget: File-backed Storage Gadget, version: 1 September 2010
UT_24] in regiong_file_storage gadget: Number of LUNs=1
 0 ...
 [c6xdspg_file_storage gadget-lun0: ro=0, nofua=0, file: /dev/sbulla
 ]  7208: SYSTEM: Creating ListMP [DSP_IPC_IN_24] in region 0 ...
 [c6xdsp ]  7208: SYSTEM: ListElem Shared Addr = 0xbea44180
 [c6xdsp ]  7210: SYSTEM: Creating ListMP [DSP_IPC_OUT_25] in region 0 ...
 [c6xdsp ]  7210: SYSTEM: Creating ListMP [DSP_IPC_IN_25] in region 0 ...
 [c6xdsp ]  7210: SYSTEM: ListElem Shared Addr = 0xbea63b80
 [c6xdsp ]  7211: SYSTEM: Creating ListMP [DSP_IPC_OUT_28] in region 0 ...
 [c6xdsp ]  7211: SYSTEM: Creating ListMP [DSP_IPC_IN_28] in region 0 ...
 [c6xdsp ]  7211: SYSTEM: ListElem Shared Addr = 0xbea83580
 [m3video]  7410: SYSTEM  : System Video Init in progress !!!
 [c6xdsp ]  7212: SYSTEM: Creating ListMP [DSP_IPC_OUT_29] in region 0 ...
 [c6xdsp ]  7212: SYSTEM: Creating ListMP [DSP_IPC_IN_29] in region 0 ...
 [c6xdsp ]  7212: SYSTEM: ListElem Shared Addr = 0xbea9d200
 [c6xdsp ] !!WARNING.Resource already registered:2
 [c6xdsp ]  7212: SYSTEM  : Initializing Links !!! 
 [m3video]  7410: SYSTEM  : System Video Init Done !!!
 [c6xdsp ]  7213: SYSTEM  : FREE SPACE : System Heap      = 6282544 B, Mbx = 10240 msgs) 
 [m3video]  7411: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_0] in region 0 ...
 [m3video]  7411: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_0] in region 0 ...
 [m3video]  7411: SYSTEM: ListElem Shared Addr = 0xbeab6e80
 [m3video]  7414: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_1] in region 0 ...
 [m3video]  7414: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_1] in region 0 ...
 [m3video]  7415: SYSTEM: ListElem Shared Addr = 0xbeaba380
 [c6xdsp ]  7229: SYSTEM  : Initializing Links ... DONE !!! 
 [m3video]  7426: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_28] in region 0 ...
 [m3video]  7427: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_28] in region 0 ...
 [c6xdsp ]  7229: SYSTEM  : System DSP Init Done !!!
 [m3video]  7427: SYSTEM: ListElem Shared Addr = 0xbeabd880
 [m3video]  7429: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_29] in region 0 ...
 [m3video]  7430: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_29] in region 0 ...
 [m3video]  7430: SYSTEM: ListElem Shared Addr = 0xbead7500
 [m3video]  7432: HDVICP: Doing PRCM for IVAHD[0] ... 
 [m3vpss ]  7434: SYSTEM  : FVID2 Init in progress DONE !!!
 [m3video]  7432: HDVICP: PRCM for IVAHD[0] ... DONE.
 [m3vpss ]  7434: SYSTEM  : Device Init in progress !!!
 [m3video]  7433: SYSTEM  : Initializing Links !!! 
 [m3vpss ]  Iss_init called !!!!!! 
 [m3vpss ]  CPIS_init DONE !!!!!! 
 [m3video]  7433: SYSTEM  : FREE SPACE : System Heap      = 6282128 B, Mbx = 10240 msgs) 
 [m3vpss ] initPrms.isI2cInitReq = 1
 [m3video]  7434: SYSTEM  : FREE SPACE : SR0 Heap         = 14742656 B (14 MB) 
 [m3vpss ] initPrms.isI2cInitReq = 1
 [m3video]  7434: SYSTEM  : FREE SPACE : Frame Buffer     = 110100352 B (104 MB) 
 [m3vpss ]  Vps_deviceInit Daughter card not detected/connected!
 [m3vpss ]                     
Simple mixer control 'PGA',0
  Capabilities: cvolume cswitch penum
  Capture channels: Front Left - Front Right
  Limits: Capture 0 - 119
  Front Left: Capture 80 [67%] [40.00dB] [on]
  Front Right: Capture 80 [67%] [40.00dB] [on]
 [m3video]  7434: SYSTEM  : FREE SPACE : Bitstream Buffer = 62914432 B (59 MB) 
 [m3video]  7434: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
 [m3video]  7435: SYSTEM  : FREE SPACE : Tiler Buffer     = 127 B (0 MB)  - TILER OFF 
 [m3video]  7491: SYSTEM  : Initializing Links ... DONE !!! 
 [m3vpss ]  I2C2: Passed for address 0x36 !!! 
queue id:0
 [m3vpss ]  I2C2: Passed for address 0x55 !!! 
 [m3vpss ]  10162: SYSTEM  : Device Init in progress DONE !!!
 [m3vpss ]  10190: SYSTEM  : System VPSS Init Done !!!
 [m3vpss ]  10190: UTILS: DMA: HWI Create for INT62 !!!
 [m3vpss ]  10190: SYSTEM  : Initializing Links !!! 
 [m3vpss ]  10190: SYSTEM  : FREE SPACE : System Heap      = 1718872 B, Mbx = 10240 msgs) 
 [m3vpss ]  10190: SYSTEM  : FREE SPACE : SR0 Heap         = 14742656 B (14 MB) 
 [m3vpss ]  10190: SYSTEM  : FREE SPACE : Frame Buffer     = 105790336 B (100 MB) 
 [m3vpss ]  10191: SYSTEM  : FREE SPACE : Bitstream Buffer = 62914432 B (59 MB) 
 [m3vpss ]  10191: SYSTEM  : FREE SPACE : Tiler Buffer     = 127 B (0 MB)  - TILER OFF 
 [m3vpss ] Received character 't'
 [m3vpss ]  10321: SYSTEM  : Initializing Links ... DONE !!! 
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
 [m3video] Received character 't'
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
 [c6xdsp ] Received character 't'
DMA: Module install successful, device major num = 248 
DRV: Module install successful
DRV: Module built on Aug 15 2013 11:26:34 
HDMI W1 rev 4.0
HDMI CEC Spec version 1.2
I2C No Ack


ApproDrvInit: 3
Creat queue id:131076
queue id:131076


 [host]  


 [host]  ORG 0x46c00524: 0


 [host]  NEW 0x46c00524: 2


 [host]  


 [host] Application Start Completed


 [host]  0: SYSTEM: System Common Init in progress !!!


 [host]  0: SYSTEM: IPC init in progress !!!


 [host]  12: SYSTEM: CPU [DSP] syslink proc ID is [0] !!!


 [host]  12: SYSTEM: CPU [VIDEO-M3] syslink proc ID is [1] !!!


 [host]  12: SYSTEM: CPU [VPSS-M3] syslink proc ID is [2] !!!


 [host]  12: SYSTEM: CPU [HOST] syslink proc ID is [3] !!!


 [host]  12: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...


 [host]  14: SYSTEM: Creating MsgQ [HOST_MSGQ] ...


 [host]  16: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] DMA: ChannelID allocated:4
...


 [host] DMA: ChannelID allocated:10
 17: SYSTEM: Opening MsgQ [DSP_MSGQ] ...


 [host]  18: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...


 [host]  18: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...


 [host]  19: SYSTEM: Notify register to [DSP] line 0, event 12 ... 


 [host]  20: SYSTEM: Notify register to [VIDEO-M3] line 0, event 12 ... 


 [host]  20: SYSTEM: Notify register to [VPSS-M3] line 0, event 12 ... 


 [host]  21: SYSTEM: IPC init DONE !!!


 [host]  22: SYSTEM: Creating ListMP [HOST_IPC_OUT_28] in region 0 ...


 [host]  24: SYSTEM: Creating ListMP [HOST_IPC_IN_28] in region 0 ...


 [host]  26: SYSTEM: ListElem Shared Addr = 0x405bb180


 [host]  27: SYSTEM: Creating ListMP [HOST_IPC_OUT_29] in region 0 ...


 [host]  29: SYSTEM: Creating ListMP [HOST_IPC_IN_29] in region 0 ...


 [host]  31: SYSTEM: ListElem Shared Addr = 0x405d4e00


 [host]  32: SYSTEM: Creating ListMP [HOST_IPC_OUT_23] in region 0 ...


 [host]  34: SYSTEM: Creating ListMP [HOST_IPC_IN_23] in region 0 ...


 [host]  36: SYSTEM: ListElem Shared Addr = 0x405eea80


 [host]  37: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ...


 [host]  39: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ...


 [host]  40: SYSTEM: ListElem Shared Addr = 0x4060e480


 [host]  41: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...


 [host]  43: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...


 [host]  45: SYSTEM: ListElem Shared Addr = 0x4062de80


 [host]  46: SYSTEM: System Common Init Done !!!


 [host] Vsys_allocBuf - addr = 0x4d1fb000,size = 65011712


 [host] MCFW_IPCBITS:App_streamSysInit:virt addr of 85000000 cir buffer  is 4d1fb000
##########pInfo->totalsize 63897600


 [host] MemMng_memcpy_open:OSA_dmaOpen passed with ch id = 4


 [host] CacheMng_MemCpy_open:OSA_dmaOpen passed with ch id = 10
queue id:131076
queue id:65538


 [host] MCFW_IPCBITS:App_ipcBitsRecvStreamFxn:Entered...queue id:0
queue id:32769


 [host] MCFW_IPCFRAMES:App_ipcFramesSendRecvFxn:Entered...

 [host] Before System_linkControl SYSTEM_M3VPSS_CMD_GET_DISPLAYCTRL_INIT


 [host] 
********** FULL FEATURE USECASE ********


 [host] ********* Entered Tri Streaming usecase - H264 1080p @60fps + H264 D1 @30fps + MJPEG 1080p @5fps ********



 [host]  133: MCFW  : CPU Revision [ES2.1] !!! 



 [host]  133: MCFW  : Detected [UNKNOWN] Board !!! 



 [host]  133: MCFW  : Base Board Revision [REV A] !!! 

 [m3vpss ] VPS_DCTRL_INST_0
 [m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_OUTPUT SYSTEM_DC_VENC_DVO2
 [m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_OUTPUT SYSTEM_DC_VENC_HDMI
 [m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_OUTPUT SYSTEM_DC_VENC_SD
 [m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_CLK_SRC VPS_DC_VENC_HDMI | VPS_DC_VENC_DVO2
 [m3vpss ]  11883: CAMERA: Create in progress !!!
 [m3vpss ]  11883: CAMERA: VIP0 PortA camera mode is [ 8-bit, Non-mux Embedded Sync] !!! 
 [m3vpss ]  11893: CAMERA: VIP 0: VID DEC 268436736 (0x36): bebebebe:bebebebe:8ebd60d8, AUD_STATUS -1094795586
 [m3vpss ] Stream ID 0: chId = 0 VpsUtils_queCreate.
 [m3vpss ] Stream ID 1: chId = 0 VpsUtils_queCreate.
 [m3vpss ]  12101: CAMERA: Create Done !!!
 [m3vpss ]  12189: CAMERA: Detect video in progress !!!
 [m3vpss ]  12189: CAMERA: Detect video Done !!!
 [m3vpss ]  12189: VNF: 
 [m3vpss ] Create in progress ... !!!
 [m3vpss ]  12190: VNF: 
 [m3vpss ] Input Channel CH0 of 1952 x 1112, pitch = (1984, 1984) [0,0][PROGRESSIVE] [7] ... 
 [m3vpss ]  12441: VNF: 
 [m3vpss ] Create ... DONE !!!
 [m3vpss ]  12537: DUP   : Create Done !!!
 [m3vpss ]  12543: DUP   : Create Done !!!
 [m3vpss ]  12545: MERGE   : Create Done !!!
 [m3vpss ] DCC server task running 
 [m3vpss ] {SWOSD} edma3Handle->tccVal = 36 
 [m3vpss ] {SWOSD} edma3Handle->chId   = 36 
 [m3vpss ] {SWOSD} edma3Handle->tccVal = 37 
 [m3vpss ] {SWOSD} edma3Handle->chId   = 37 
 [m3vpss ] {SWOSD} edma3Handle->tccVal = 38 
 [m3vpss ] {SWOSD} edma3Handle->chId   = 38 
 [m3vpss ]  12520: SWOSD   : Create Done !!!
 [m3vpss ]  12616: DUP   : Create Done !!!
 [m3vpss ]  12616: SCLR: Create in progress !!!
 [m3vpss ]  12638: SCLR    : Loading Up-scaling Co-effs ... 
 [m3vpss ]  12638: SCLR    : Co-effs Loading ... DONE !!!
 [m3video]  12657: IPC_IN_M3   : Create in progress !!!
 [m3vpss ] SCLR:HEAPID:0	USED:64
 [m3video]  12657: SYSTEM: Opening ListMP [VPSS-M3_IPC_OUT_0] ...
 [m3vpss ] SCLR:HEAPID:1	USED:5952
 [m3video]  12657: SYSTEM: Opening ListMP [VPSS-M3_IPC_IN_0] ...
 [m3vpss ]  12639: SCLR: Create Done !!!
 [m3video]  12660: IPC_IN_M3   : Create Done !!!
 [m3vpss ]  12565: FD   : Alg Create Done !!!
 [m3video]  12661: ENCODE: Create in progress ... !!!
 [m3vpss ]  12565: FD   : Create Done !!!
 [m3vpss ]  12655: IPC_OUT_M3   : Create in progress !!!
 [m3vpss ]  12656: IPC_OUT_M3   : Create Done !!!
 [m3video]  12724: ENCODE: Creating CH0 of 1920 x 1080, pitch = (1952, 1952) [PROGRESSIVE] [NON-TILED  ], bitrate = 8000 Kbps ... 
 [m3video] ENCLINK_H264:HEAPID:0	USED:13808
 [m3video]  12831: ENCODE: Creating CH1 of 720 x 480, pitch = (720, 720) [PROGRESSIVE] [NON-TILED  ], bitrate = 8000 Kbps ... 


 [host] IpcBitsInLink_tskMain:Entered

 [host]  1112: IPC_BITS_IN   : Create in progress !!!


 [host]  1112: IPC_BITS_IN   : ListMPOpen start !!!


 [host]  1112: SYSTEM: Opening ListMP [VIDEO-M3_IPC_OUT_28] ...


 [host]  1114: SYSTEM: Opening ListMP [VIDEO-M3_IPC_IN_28] ...


 [host]  1116: IPC_BITS_IN   : ListMPOpen done !!!


 [host]  1117: IPC_BITS_IN   : System_linkGetInfo done !!!


 [host]  1117: IPC_BITS_IN   : Create Done !!!
 [m3vpss ]  12954: DISPLAY: Create in progress !!!
 [m3video] ENCLINK_H264:HEAPID:0	USED:11912
 [m3vpss ] DisplayId = 1,DataFormat = 7
 [m3video]  12941: ENCODE: Creating CH2 of 1920 x 1080, pitch = (1952, 1952) [PROGRESSIVE] [NON-TILED  ], bitrate = 100 Kbps ... 
 [m3vpss ] SC2 displayInstId = 6
 [m3vpss ]  12955: DISPLAY: Create Done !!!
 [m3vpss ]  12956: DISPLAY: Create in progress !!!
 [m3video] ENCLINK_JPEG:HEAPID:0	USED:4432
 [m3vpss ] DisplayId = 4,DataFormat = 7
 [m3video]  12941: ENCODE: All CH Create ... DONE !!!
 [m3vpss ] SD displayInstId = 2


 [host] USECASE SETUP DONE
 [m3vpss ]  12957: DISPLAY: Create Done !!!
 [m3video] ENCLINK:HEAPID:0	USED:30472
 [m3vpss ]  12958: DISPLAY: Start in progress !!!
 [m3video]  12944: ENCODE: Create ... DONE !!!
 [m3video]  12804: VSTAB   : Alg Create Done !!!
 [m3video]  12804: VSTAB   : Create Done !!!
 [m3video]  12945: IPC_BITS_OUT   : Create in progress !!!
 [m3video]  12948: IPC_BITS_OUT   : Create Done !!!
 [m3vpss ]  13001: DISPLAY: Start Done !!!
 [m3vpss ]  13001: DISPLAY: AUX PATH: 46 fps, Latency (Min / Max) = ( 255 / 0 ), Callback Interval (Min / Max) = ( 255 / 0 ) !!! 
 [m3vpss ]  13002: DISPLAY: Start in progress !!!
 [m3vpss ]  13065: DISPLAY: Start Done !!!
 [m3vpss ]  13065: DISPLAY: SDDAC(SEC1): 15 fps, Latency (Min / Max) = ( 255 / 0 ), Callback Interval (Min / Max) = ( 255 / 0 ) !!! 
 [m3vpss ]  12978: CAMERA: Start in progress !!!
 [m3vpss ]  12978: CAMERA: Start Done !!!


 [host] 
Application Run Completed
 [m3vpss ]  13126: CAMERA: Fields = 2 (fps = 0), Total Resets = 0 (Avg 0 ms per reset)


 [host] ITT server task running !!!


 [host] 
 ITT ittServer_run


 [host] ITT Server Message initialization successful


 [host] 
 ITT capture task created


 [host] DCC server Message ques is open succefully


 [host] Setting cmd <1> in message <403d5100>


 [host] Posting message <403d5100> in QId <20002> 
 [m3vpss ] Command 1 recived from HOST A8 


 [host] Response from M3 is : 1


 [host] Response from M3 is : 1


 [host] Default parameters were sent sucessfully 


 [host] Server Socket created with ID <22> 
 [m3vpss ] Command 2 recived from HOST A8 
 [m3vpss ] New DCC data of size <33603> 
 [m3vpss ] Call to VNF_LINK_CMD_UPDATE_DCC 536870977
queue id:0
ApproDrvInit: 10
queue id:131076
Initializing...
...done initializing
ApproDrvInit: 6
queue id:131076
Initializing...
ApproDrvInit: 2
queue id:131076
Initializing...
...done initializing
ApproDrvInit: 9
queue id:131076
Initializing...
...done initializing
...done initializing
ApproDrvInit: 8
queue id:131076
Initializing...
...done initializing
Play this stream using the URL:
	Play this stream using the URL:
	rtsp://0.0.0.0:8554/PSIA/Streaming/channels/1?videoCodecType=MPEG4

(We use port 8301 for optional RTSP-over-HTTP tunneling.)
Play this stream using the URL:
	rtsp://0.0.0.0:8556/PSIA/Streaming/channels/2?videoCodecType=H.264

(We use port rtsp://0.0.0.0:8553/PSIA/Streaming/channels/1?videoCodecType=MPEG4

(We use port 8300 for optional RTSP-over-HTTP tunneling.)
8303 for optional RTSP-over-HTTP tunneling.)
Play this stream using the URL:
	rtsp://0.0.0.0:8557/PSIA/Streaming/channels/2?videoCodecType=H.264

(We use port 8304 for optional RTSP-over-HTTP tunneling.)
Play this stream using the URL:
	rtsp://0.0.0.0:8555/PSIA/Streaming/channels/0?videoCodecType=MJPEG

(We use port 8302 for optional RTSP-over-HTTP tunneling.)
ApproDrvInit: 7
queue id:131076
TimeOut occure in boot_proc.
Program exit.
TimeOut occure in boot_proc.
Program exit.


 [host] 
Usecase is Active !!! 
ApproDrvExit: 7
Error: WaitStreamReady Fail.
Error: SemWait: Invalid Semaphore handler

would someone give me some advice to solve the issue?

thank you.

  • Hi Simon,

    If below is the error part which you are reffering to, then  I have some suggestions for you.

    (We use port 8302 for optional RTSP-over-HTTP tunneling.)
    ApproDrvInit: 7
    queue id:131076
    TimeOut occure in boot_proc.
    Program exit.
    TimeOut occure in boot_proc.
    Program exit.
       [host]  
    Usecase is Active !!!  
    ApproDrvExit: 7
    Error: WaitStreamReady Fail.
    Error: SemWait: Invalid Semaphore handler

    • Do a CLEAN BUILD. using make -s clean and make -s sysall
    • after booting the IPNC with fresh build,  execute below Command.
      rm -rf /mnt/nand/*
    • Restart the board after step 1  & 2. Now you should be able to see the streams without any issue !!
  • thank your timely response.

    Unfortunately,the issue still remain after the recommended solution steps.

    now,i suspect something configuration about DCC defaulty data communication between A8 and VPSS M3 are missing from the log information:

     boot_proc Time out and Error: WaitStreamReady Failure ofen comes after this:

    [m3vpss ] Command 2 recived from HOST A8
     [m3vpss ] New DCC data of size <33603>
     [m3vpss ] Call to VNF_LINK_CMD_UPDATE_DCC 536870977

    If this is ture,please give me some clue about that.

    thank you again.

     

     

  • Hi,ravikiran

    Now,for the above reason.

    i can't get video stream .samely,can't set the streams types , numbers and so on.

    how to pass parameters to ipnc_rdk_mcfw.out 's main entry?except edit code of ti_mcfw_ipnc_main.c.

    for example:./bin/ipnc_rdk_mcfw.out   VA SNF TNF VNF_QUALITY DUALSTREAM H264_JPEG APPRO2A AEWB 1080P_D1 H264 HIGH_SPEED1 MJPEG 80 &

    maybe the above issue is caused by the parameters of ipnc_rdk_mcfw.out.because in the multich_tristream_fullfeature.c,code always runs into else branch

    if(Vsys_getSystemUseCase() == VSYS_USECASE_TRISTREAM_SMARTANALYTICS)
     {
      OSA_printf("\n********** SMART ANALYTICS USECASE ********\n");
      OSA_printf
       ("********* Entered Smart Analytics usecase - H264 1080p @60fps + H264 D1 @30fps + MJPEG 1080p @5fps ********\n\n"); 
     }
     else
     {
      OSA_printf("\n********** FULL FEATURE USECASE ********\n");
      OSA_printf
       ("********* Entered Tri Streaming usecase - H264 1080p @60fps + H264 D1 @30fps + MJPEG 1080p @5fps ********\n\n");
     } 

    thank you.