This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Status of NAND driver (8-bit ECC & DMA) in linux branch

Would be great if we could get 8-bit ECC support as well as the DMA-tweaks/speed-ups discussed here: AM335x NAND prefetch engine: speed breakdown due to data cache writeback integrated into the main TI linux branch.

The industry seems to move from 34nm to 25nm NAND's like MT29F2G08ABAFAH4:F this will also switch from 4-bit ECC to 8-bit. 

Another question, Micron still has some nands with "on-die ECC". Any thoughs on how this would perform vs the AM335x GPMC. 

best david