Hi,
The hardware I am using is DM8148 EVM with Vision application board. Both u-boot and RPRC image are flashed into NOR flash successfully.
The problem occurs when jumping to the entry point of application. The PC falls into an unknown address 0x2008C.
I am sure that the content of RPRC image is completed copied into DDR, because I already checked the content in DDR is the same as the image.
Currently, I really have no idea why the CPU hangs. Can someone provide any thoughts or tips, please?
Thanks and regards,
Kershaw