This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM1808 EVM build environment

Other Parts Discussed in Thread: AM1808, OMAP-L138

I'm trying to follow the following instruction: 

http://arago-project.org/wiki/index.php/Setting_Up_Build_Environment

When I execute oe-layertool-setup.sh, 
what configuration should I choose for AM1808EVM?   

The config for latest SDK, 6.0 seems to be config/amsdk-06.00.00.00-config.txt, but is this compatible with AM1808? 

It doesn't seems so because it does include reference to meta-linaro and ARM9 is not supposed to be compatible with it. 

What is the version of SDK compatible with AM1808, or is there recipe to make 6.0 work with AM1808?