This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About MJPEG encode quality



Hello,

We are using DVR RDK 4.0 and we found that the image quality after MJPEG encoding is not good as we expected.

And I had searched the related post on forum, it said that I need to modify the targetbitrate and qpInit.

Here is my configuration to these two options:

Resolution: 1920x1080

targetBitRate: 1000*1000  (1Mbps)

qpInit: 2  (2~97, I choose 2, is it referred to the best quality?)

But I still see the obviously coding artifact, is there any parameter I can tune to further improve the quality?

Please see the attachment, and see the time digit in the down-left.

Thanks,

Thorpe