This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to create shared heap in msgCom unit test sample



Development environment: CCS 5.4 with SC-MCSDK 2_01_00_01

Target: TCI6614

There are some msgCom unit test projects created in SYSLIB folder.

I tried to run the msgCom unit test for DSP Core to DSP Core.

The following two project are loaded into Core0 and Core1.

1.Core0_msgCom_tmdxevm6614lxe_UnittestProject_little

2.Core1_msgCom_tmdxevm6614lxe_UnittestProject_little

While the Core0 is started after Core1 is started, the output message from the console is as below:

--

[C66xx_0] ***********************************
**** Message Communicator Test ****
***********************************
Debug: RM Initialization was successful
Debug: Inserting MSMC Memory Region (Core0-MSMC) @ Index 0 Start Index 0
Debug: Inserting LOCAL Memory Region (Core0-Local) @ Index 1 Start Index 128
Debug: Inserting LOCAL Memory Region (Core1-Local) @ Index 2 Start Index 256
Debug: Inserting DDR3 Memory Region (Core1-DDR3) @ Index 3 Start Index 384
Debug: RM LLD Revision: 01.00.00.15:Mar 26 2013:17:03:10
Debug: QMSS LLD Revision: 01.00.03.20:Mar 26 2013:17:02:56
Debug: CPPI LLD Revision: 01.00.02.04:Mar 26 2013:17:02:34
Error: Unable to create shared heap error code -3
[C66xx_1] Debug: RM Startup was successful

--

The error is caused by Pktlib_createHeap() function and the error code -3 means there was a resource error.

Would anyone know what the problem is, thanks in advance!

--

/* A part of main_core0.c */

/* Initialize the Shared Heaps. */
result = Pktlib_sharedHeapInit();
if(result < 0)
{
System_printf ("Error: Pktlib_sharedHeapInit %d\n", result);
return -1;
}

/* Initialize the heap configuration. */
memset ((void *)&heapCfg, 0, sizeof(Pktlib_HeapCfg));

/* Populate the heap configuration */
heapCfg.name = "MySharedHeap";
heapCfg.memRegion = ptrCfg->memRegionResponse[0].memRegionHandle;
heapCfg.sharedHeap = 1;
heapCfg.useStarvationQueue = 0;
heapCfg.dataBufferSize = TEST_MAX_DATA_SIZE;
heapCfg.numPkts = 64;
heapCfg.numZeroBufferPackets= 0;
heapCfg.dataBufferPktThreshold = 0;
heapCfg.zeroBufferPktThreshold = 0;
heapCfg.heapInterfaceTable.data_malloc = mySharedMemoryMalloc;
heapCfg.heapInterfaceTable.data_free = mySharedMemoryFree;

/* Create the Heap. */
mySharedHeapHandle = Pktlib_createHeap(&heapCfg, &errCode);
if (mySharedHeapHandle == NULL)
{
System_printf ("Error: Unable to create shared heap error code %d\n", errCode);
return -1;
}

--

Kenny

  • Kenny,

    TCI66xx devices are only supported through your local Field Applications Engineers (FAE.)  They are not supported on the forum.  Please contact your local FAE for direct support of TCI66xx devices.  If you do not know who your local FAE is, then please contact your local TI field sales person and they would be able to put you in touch with your local FAE.  

    Best Regards,

    Chad