This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB Webcam with OMAP-L138 LCDK

Other Parts Discussed in Thread: OMAP-L138, OMAPL138

Hello,

I am very new to embedded platforms.

I am trying to use a  Microsoft® LifeCam HD-3000 usb webcam to capture video on the OMAP-L138 LCDK board. My initial goal is to simply capture video using the webcam and output the video to a monitor using the vga port. I am using Code Composer Studio 5.4.0 with an XDS100v2 JTAG emulator to test the programs. I am also able to use Tera Term to view the Linux system on the board

When I am using Tera Term and I have booted up the board, I can plug in the webcam and the following output occurs:

root@omapl138-lcdk:~# usb 1-1: new full speed USB device number 4 using ohci
usb 1-1: New USB device found, idVendor=045e, idProduct=0779
usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
usb 1-1: Product: Microsoft® LifeCam HD-3000
usb 1-1: Manufacturer: Microsoft

I guess my question are as follows:

-How do I control the webcam?

-How do I take the captured images and output them via the VGA port?

-Is there example code capturing video using a USB webcam? (I have searched extensively and not found anything I recognized as useful).

Thank you very much in advance for any help!