Other Parts Discussed in Thread: TFP410, TVP7002
Application:
This is a PC-graphics only application and we only need to support the 15 formats listed at the top of the spread sheet.
We are using an external 27 MHz clock.
Q1. Is there a tolerance for the lines per frame and clocks per line?
Q2. Is the write-up, section 3 correct?
Q3. Since this is a PC-graphics only application which I2C sub-address registers can be ignored?