This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Packet Accelerator issues

Hi
    
    I have some questions about Packet Accelerator on keystone device(take tci6614 for example)
    
    I'm writing an ethernet driver which will run on the ARM core of keystone, I see the training of netcp&pa, one step of PA configaration is loading the firmware to the PDSP.
    
    so my questions:
    
    1.Is the loading of firmware necessary for my driver? My driver will just support some simple ethernet functions, for example:adding mac addr(Adding Entries to the L2 Classification Engine) to match the incoming packages and using modify engines to generate some checksum.
    2.if the loading of firmware is necessary, how can I get the firmware files? And can you please provide some reference code for downloading the firmware file?
    
    Thanks?

  • TCI66xx devices are supported through Field Applications Engineers (FAEs)  TCI66xx devices are not supported on the E2E forum.  Please work with you local FAE for support of TCI6614 devices.  If you do not know who your local FAE is then please contact your local field sales representative and they would be happy to put in contact with your local FAE.

    Best Regards,
    Chad