Does DM814x support SDHC "UHS-1" memory card?
There was an issue with "TS32GUSDCU1" Transcend's memory model.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does DM814x support SDHC "UHS-1" memory card?
There was an issue with "TS32GUSDCU1" Transcend's memory model.
Hi Hayden,
I think "UHS-1" is the same as "UHS-I", right?
It seems that DM814x/AM387x device does not support SDHC UHS-I cards. See the thread below:
https://e2e.ti.com/support/dsp/davinci_digital_media_processors/int-dm814x/f/720/t/96406.aspx
We do support SDHC cards – and we have specifically tested with the max.capacity of 32GB.
The device supports SDHC cards with the limitation listed below, but it doesn't support boot from SDXC cards.
Card types:
Non UHS-I card: supported
UHS50 card: supported
UHS104 card: supported, but SDR104 speed bus mode not supported
BR
Pavel