This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM37xx Advisory 1.113 - workaround -> TUSB2036?

Expert 3020 points

Other Parts Discussed in Thread: TUSB2036

Hello,

The proposed work around for advisory 1.113 is a USB hub chip.

From the Errata:

Advisory 1.113 USB HOST:
Impossible To Attach a FS Device To An EHCI Port - Handoff To OHCI Is Not Functional
Revision(s) Affected 1.2, 1.1 and 1.0

Workaround(s) Only attach FS devices to OHCI ports or use an HS hub to interface between EHCI ports
and LS/FS/HS devices.

If I only want to connect (and hotplug) USB 1.1 devices, would the TUSB2036 (without EEPROM) be a good choice?

http://www.ti.com/product/tusb2036

Regards,

Lo

Advisory 1.113 USB HOST:
Impossible To Attach a FS Device To An EHCI Port - Handoff To OHCI Is Not Functional
Revision(s) Affected 1.2, 1.1 and 1.0