Hey Guys,
i tried to connect dcan to the EVM. So i changed the EVM Profile from 0 to 1, as its described in the hardwareguide and the dcan driver guide:
http://processors.wiki.ti.com/index.php/AM335X_DCAN_Driver_Guide#Port_details
http://processors.wiki.ti.com/index.php/AM335x_General_Purpose_EVM_HW_User_Guide#Configuration.2FSetup
After this i connect an USB-to-CAN Adapter to the J11 DCAN on the daughter board. And booted the board.
But the board wasnt booting anymore. Only the LED on the LCD Board is activ. The daughterboards LEDs arent activ and no UART Output is printed to my console. I think i crashed the board cause i turned back to the initial options (profile 0, mmc boot), but nothing works now.
did i crashed the board? or did i flashed the cpld by switch to profile 1?
best regards and thanks for the help,
al.