This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM642 - PCI Slave Read - similar DSPvd03632 but with 4 bytes to read

Have similar issues to DSPvd03632.

Host read\writes data from\to DM642's external SDRAM. Suddenly host may totally stuck. 

By scope it looks like host trying to read form DM642 4 bytes (/BE3-0 are 0), gets retry form DSP, and repeats - so gets deadlock.

DSP core is running - can see leds flashing. Also can connect via JTAG. Seems DSP works fine. But deadlock exists.

If I do DSP reset via CCS - the host continue to work fine :S

 

What can it be? Please advice.