This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467 H264 Decoder



I'm trying to create an application that decodes and displays a signal but the image appears blurry.  I decode frames until outArgs.outputID[ 0 ] > 0.  Then I pass the value in outArgs.displayBufs[ 0 ].bufDesc[ 0 ].buf to address.buffers[ VDCE_BUF_IN ].virt_ptr and do a chroma conversion.  The outArgs.displayBufs[ 0 ].frameWidth and frameHeight are 720 x 480, which is what I'm trying to display.  The framePitch is 768.  If I use this value for address.src_horz_pitch, the VDCE_START ioctl returns an invalid size error.  Any suggestions where I'm going wrong?