I use AER_16_1_0_3 software to remover acoustic echo.CPu is C6748.But I meet some trouble with it.
When I disable AER,the speaker can play the voice from the far end and the microphone can pick up the voice and sent to the far end.But when I enable AER,the speaker can play the voice and the far end voice is very serious attenuation.The AER is running in hand free mode.In my code ,the bitfield_0 is 0x188f,the bitfield_1 is 0x01ce.
How can I do to save the problem.Thanks a lot.