This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ti.sysbios.knl.Semaphore: line 207: assertion failure: A_badContext: bad calling context

Hi all,

DSP: 6670

BIOS: 6_35_01_29

I run a GPIO-test project with bios, and go to such a abort with log after runing for about 3 minutes :

[ti.sysbios.knl.Semaphore: line 207: assertion failure: A_badContext: bad calling context,Must be calling from a task, xdc.runtime.Error.raise:terminating execution.]

also warning from the edit window:

"Can't fimd a source file at"/temp/TI_MKLIB6sLCzz/SRC/exit.c" Locate the file or edit the source lookup path to include its location."

I have no idea how to debug......

Appreciate your attention and help!

Frank