Hi, all
I have the following requirements:
1, want to connect ADC to C6655 directly;
2, ADC specification: 2 channel, 14bits, 100MHz sampling rate
Can I connect ADC to C6655 uPP? I'm not sure weather the max data rate of uPP can satisfy the requirement . The uPP user's guide has the following description: ".... I/O speed up to 75MHz with 8-16 bit data width with per channel....."
would you please give me some suggestions?
Thanks a lot
Mosha