This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

rdk myown osd test runtime error



hi all .when i run my test application as the first time ,it is normal . but when i stop the application,then run the application or other applications again, it will occur following error. so who can tell me what about the error.

tks

 

 =========
 Main Menu
 =========

 1: VCAP + VENC + VDEC + VDIS  - Progressive SD Encode + Decode
 2: VCAP + VENC        + VDIS  - SD Encode ONLY
 3: VCAP + VENC + VDEC + VDIS  - Progressive HD Encode + Decode
 4:               VDEC + VDIS  - SD/HD Decode ONLY
 a: 960H DVR usecase

 e: Exit

 Enter Choice: 1
--------------- CHANNEL DETAILS-------------
Capture Channels => 2
Enc Channels => Primary 2, Secondary 0
Dec Channels => 2
Disp Channels => 4
-------------------------------------------
 0: SYSTEM: System Common Init in progress !!!
 0: SYSTEM: IPC init in progress !!!
 12: SYSTEM: CPU [DSP] syslink proc ID is [0] !!!
 12: SYSTEM: CPU [VIDEO-M3] syslink proc ID is [1] !!!
 12: SYSTEM: CPU [VPSS-M3] syslink proc ID is [2] !!!
 12: SYSTEM: CPU [HOST] syslink proc ID is [3] !!!
 12: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_3] ...
 15: SYSTEM: Creating MsgQ [HOST_MSGQ] ...
 16: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ...
 18: SYSTEM: Opening MsgQ [DSP_MSGQ] ...
 18: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...
 19: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
 20: SYSTEM: Notify register to [DSP] line 0, event 15 ...
 21: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ...
 21: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ...
 22: SYSTEM: IPC init DONE !!!
 23: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ...
 25: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ...
 26: SYSTEM: ListElem Shared Addr = 0x406b7b00
 27: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...
 30: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...
 31: SYSTEM: ListElem Shared Addr = 0x406ecd00
 33: SYSTEM: Creating ListMP [HOST_IPC_OUT_19] in region 0 ...
 35: SYSTEM: Creating ListMP [HOST_IPC_IN_19] in region 0 ...
 36: SYSTEM: ListElem Shared Addr = 0x40764f80
 37: SYSTEM: Creating ListMP [HOST_IPC_OUT_20] in region 0 ...
 40: SYSTEM: Creating ListMP [HOST_IPC_IN_20] in region 0 ...
 41: SYSTEM: ListElem Shared Addr = 0x407a8280
 42: SYSTEM: Creating ListMP [HOST_IPC_OUT_21] in region 0 ...
 44: SYSTEM: Creating ListMP [HOST_IPC_IN_21] in region 0 ...
 ASSERT (system_ipc_listMP.c|System_ipcListMPAllocListElemMem|211)