During initialization and first interrupt, one buffer size is needed. However, after that, ideally, it would be required to change the buffer size to line up interrupts with incoming data stream.
Can the buffer size for a transmit DMA and receive DMA be changed after the first interrupt?
This would be set up to overcome the errata for I2S "Transmit Path Internal Delays" and DMA "Receive Path Internal Delays."