Hi,
after setting up the board I'm trying to start working on it.
First of all I've launched the demos but only the "decode" demo works. That's because I've a PAL camera. I've changed the J1 jumper and set the bootargs accordingly to the instructions I've read on the GSG and on some threads here on the forum: no results. The ntsc mode is always selected. What's the matter? I always get "PAL camera connected but NTSC selected"...
videostd variable is correctly set by J1 as "pal"
My bootargs are:
bootargs=console=ttyS0,115200n8 noinitrd rw ip=192.168.10.11:192.168.10.10:192.168.10.1:255.255.255.0:::off root=/dev/nfs nfsroot=192.168.10.10:/home/ns/workdir/filesys,nolock mem=116M video=davincifb:vid0=720x576x16,2500K:vid1=720x576x16,2500K:osd0=720x576x16,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=pal
Second (and most important) point:
I've compiled and run the "Hello world!" program using the arm gcc but, since I'm not a linux geek, I hoped to have an IDE included in the box (as Microchip, Atmel, Rabbit, Cyan tech. do) which could lead me from very basics.
I cannot understand where is it. I read, on some threads, about commercial tools but, as I'm evaluating the product, I'd prefer not to spend more money before I decide if the 355 is what I'm looking for (BTW I think this is the aim of eval boards...).
Thanks,
s.