Team,
Could you please confirm the following?
There are some support for short circuit detection on the DM365 TVOUT pin of the DAC. So looking at the description provide in SPRUFG9A it looks like that you can detect the short circuit via VDAC_CONFIG.TVSHORT and VDAC_CONFIG.PDTVSHORTZ bit fields.
Looking at DM365 datasheet SPRS457B page 149 a video buffer can be enabled via some registers bit field.
Is it expected that this video buffer can act as protection circuit in case of short circuit on the TVOUT? If yes can the TVOUT be permanently shorten without damaging the device?
If it is suppose to protect for a short period of time do you have some timing information about it?
Thanks and BR,
A.