This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Example code for setting L1P, L1D and L2 cache on C6455.



Hi everyone,

I am looking for an example code setting L1P, L1D and L2 cache on C6455. This is what I want to do: upon the chip power-up or reset, I would like to set up the followings:

(1) L1P size to 32K

(2) L1D size to 32K

(3) L2 cache size to 256K

(4) Set up MAR to indicate which external memory addresses are cacheable

 

I have already read through this example code:

csl+3.0.10.2\csl_c6455\example\cache\src\Cache_example.c

but the example does not show the sequence of commands/functions to set up all L1 and L2 caches.