Hi,
Im trying to compile the ubl source code present in the dvsdk_4_02_00_06_dm365
I imported the project into the CCSv5 using "Project->Import Legacy CCSv3.3 Project".
then compiled it.
the issue im facing is:
error in converting the .out file to bin file. apparently the hex470.exe is not present in the ccs5.
please help
Best regards,
Nir Or