This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x SPI slave mode TX problem

I'm having an intermittent problem running the BeagleBone Black's SPI1 in slave mode.  I have designed all my TX messages to end in 0, and have verified every way I know how that the last byte written to MCSPI_TX0 is 0.  But after a few minutes of running, there is a non-zero value stuck on the output.  It is usually 0x80, (I am in 8-bit mode), and I can clearly see the 0x80 coming out of the D1 line on a scope.  The communication is very reliable initially, several messages get through OK before the error.  I have to soft reset the AM335x SPI to clear the error condition.

 Thanks,
  Jim