HI
Hope you could help, working thru some labs and want to test ssh protocol so that I can use connect with CCS
darren@darren-desktop:~$ nslookup am335x.gigether.net
Server: 192.168.0.1
Address: 192.168.0.1#53
Non-authoritative answer:
Name: am335x.gigether.net
Address: 216.21.239.197
this is lab 4 intro to embedded linux.
I can do ssh root@192.168.0.5 and connect to the board.
But I need to fix this so that I can connect with CCS. Hope you could advise.
Thank you
Darren