This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can we get the MPS430 source code on EVMDM648?

Nowadays, I am testing my dm648 board. When I burn the UBL and App program into flash, power up, the UBL can run but the App could not run. And I debug the UBL, it can copy the App code into DDR, and Jump to the new start point, and the App program can run rightly. The boot config pins are rightly configed, and the bootcfg reg is also right, I do not konw where  the problem is, so I want to get the MPS430 source code to reference the boot process. Not a long time ago, I tried to get the source code from the board maker LYRTECH, but they said that I should ask for TI. We can see there are so many people in the question about boot on e2e forum, but we can not get the answer rightly. The dm648 and the EVM are very excellent designs, and thip chip is fit to our need, we will feel very grateful if you could show us the source code.
thank you!
zhuyh