This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About IBL for C6670

Guru 15520 points

Hi,

I have a question about C6670 boot.

I'm planning to connect NOR Flash via SPI,
and going to use SPI boot.

I understand that IBL is needed if application image are
flashed in the NOR/NAND(which is connected via EMIF),
because C6670 doesn't support EMIF boot.

But in our case(SPI boot), do I need to use IBL?
If it is true, do I need to implement I2C EEPROM to our board
and flash IBL to this I2C EEPROM?

best regards,
g.f.