I have two clarification on the PMIC .
- On page 7 of SWCU093C, the sleep signal and INT signals are connected to GPIO1-9 and 8 respectively, Is there a particular reason for choosing this specific IO? Any problem if we assigned to other IO?
- We have chosen TPS65910A31A1, which is a high power mode device. We are planning to use the RTC in PMIC, If we use the low power mode device, will we be able to use the PMIC RTC without any constraints?
Thanks.