This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

venc-secondary stream?

Hello,TI man.

We use Dm8168 in our box.If we wanna generate secondary stream by M3 codec.Can M3 codec output Low resolution,full FPS video stream?

BR.

  • Your question is not clear. Does your data flow scale the captured  image into two resolutions ? Secondary stream encoding is supported and is enabled in following usecases. Whether you will be able to achieve full fps secondary stream encoding depends on the number of channels you are encoding.

    /dvr_rdk/mcfw/src_linux/mcfw_api/usecases/ti816x/multich_progressive_vcap_venc_vdec_vdis.c

    /dvr_rdk/mcfw/src_linux/mcfw_api/usecases/ti816x/multich_hybrid_encode.c

    /dvr_rdk/mcfw/src_linux/mcfw_api/usecases/ti816x/multich_hybrid_dvr.c

    /dvr_rdk/mcfw/src_linux/mcfw_api/usecases/ti816x/multich_vcap_venc_vdis.c

    /dvr_rdk/mcfw/src_linux/mcfw_api/usecases/ti816x/multichhd_vcap_venc_vdis.c

  • Sorry for my bad descriptions.

    I mean that If JUST send ONE HIGH resolution,FULL fps video frame to M3 codec WITHOUT sending a same content,low resolution,full fps video frame to M3 codec.

    Can M3 codec output two video stream?One PRIMARY stream,HIGH resolution,FULL fps.and secondary stream is low resolution,full fps stream.

  • No such a  feature is not supported. The h264 encoder in DVR RDK supports SVC-T which means same stream can have multiple layers with each layer having lower FPS but all have the same resolution.

  • Thank you,I know that.