This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

With the CE development, DM6446. We first use of G711DEC routines, bringing in the DVSDK G711 all of the code



With the  CE development, DM6446. We first use of G711DEC routines, bringing in the DVSDK G711 all of the code. Using CCS5.3 compiler generates the lib files. Then using genpackage and genserver wizard generated codecs and the servers

But ARM call again. In the audio decoder card. At that time the ARM CPU LOAD10% DSP 80%. Audio rate also has a problem. The DEMO application G711codecs ARM CPU LOAD DSP4%4% at runtime

why