Dear manager,
Now I use beaglebone black with kernel 3.2.0 and arogo file system from TI SDK 06.00.00.00. The information of start is as following:
U-Boot 2013.01.01 (Jun 25 2013 - 16:42:52)
I2C: ready
DRAM: 512 MiB
WARNING: Caches not enabled
NAND: No NAND device found!!!
0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw, usb_ether
Hit any key to stop autoboot: 0
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
** Unable to read file uEnv.txt **
reading uImage
** Unable to read file uImage **
3202144 bytes read in 335 ms (9.1 MiB/s)
Booting from mmc ...
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Linux-3.2.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3202080 Bytes = 3.1 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
XIP Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0 (root@guocs-desktop) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #4 Mon Sep 2 12:45:07 CST 2013
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES2.0 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext3 rootwait ip=none
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 512MB = 512MB total
[ 0.000000] Memory: 513152k/513152k available, 11136k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc059c000 (5712 kB)
[ 0.000000] .init : 0xc059c000 - 0xc05d7000 ( 236 kB)
[ 0.000000] .data : 0xc05d8000 - 0xc0642630 ( 426 kB)
[ 0.000000] .bss : 0xc0642654 - 0xc0671424 ( 188 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000061] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.089233] pid_max: default: 32768 minimum: 301
[ 0.089324] Security Framework initialized
[ 0.089385] Mount-cache hash table entries: 512
[ 0.089691] CPU: Testing write buffer coherency: ok
[ 0.108947] omap_hwmod: pruss: failed to hardreset
[ 0.109863] print_constraints: dummy:
[ 0.110137] NET: Registered protocol family 16
[ 0.111755] OMAP GPIO hardware version 0.1
[ 0.113708] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.115142] omap_i2c.1: alias fck already exists
[ 0.115814] omap2_mcspi.1: alias fck already exists
[ 0.115997] omap2_mcspi.2: alias fck already exists
[ 0.116668] edma.0: alias fck already exists
[ 0.116699] edma.0: alias fck already exists
[ 0.116699] edma.0: alias fck already exists
[ 0.136322] bio: create slab <bio-0> at 0
[ 0.138000] SCSI subsystem initialized
[ 0.139251] usbcore: registered new interface driver usbfs
[ 0.139495] usbcore: registered new interface driver hub
[ 0.139648] usbcore: registered new device driver usb
[ 0.139892] registerd cppi-dma Intr @ IRQ 17
[ 0.139892] Cppi41 Init Done Qmgr-base(e087a000) dma-base(e0878000)
[ 0.139892] Cppi41 Init Done
[ 0.139923] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.140167] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.141021] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.142059] tps65910 1-002d: could not be detected
[ 0.143066] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.143920] Switching to clocksource gp timer
[ 0.155364] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.155517] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.155792] MUSB0 controller's USBSS revision = 4ea20800
[ 0.155822] musb0: Enabled SW babble control
[ 0.156555] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using DMA, IRQ 18
[ 0.156677] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.156921] MUSB1 controller's USBSS revision = 4ea20800
[ 0.156951] musb1: Enabled SW babble control
[ 0.157257] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.157348] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.157440] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.157440] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.157470] usb usb1: Product: MUSB HDRC host driver
[ 0.157470] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[ 0.157470] usb usb1: SerialNumber: musb-hdrc.1
[ 0.158142] hub 1-0:1.0: USB hub found
[ 0.158172] hub 1-0:1.0: 1 port detected
[ 0.158569] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using DMA, IRQ 19
[ 0.158905] NET: Registered protocol family 2
[ 0.159057] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.159271] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[ 0.159484] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.159637] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.159637] TCP reno registered
[ 0.159637] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.159667] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.159820] NET: Registered protocol family 1
[ 0.160003] RPC: Registered named UNIX socket transport module.
[ 0.160034] RPC: Registered udp transport module.
[ 0.160034] RPC: Registered tcp transport module.
[ 0.160034] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.160217] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.177062] VFS: Disk quotas dquot_6.5.2
[ 0.177124] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.177520] msgmni has been set to 1002
[ 0.179962] alg: No test for stdrng (krng)
[ 0.180480] io scheduler noop registered
[ 0.180480] io scheduler deadline registered
[ 0.180541] io scheduler cfq registered (default)
[ 0.181457] Could not set LED4 to fully on
[ 0.214813] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.795501] console [ttyO0] enabled
[ 0.799621] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.807373] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.815063] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.822723] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.830413] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 0.838470] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
[ 0.852294] brd: module loaded
[ 0.859191] loop: module loaded
[ 0.862609] i2c-core: driver [tsl2550] using legacy suspend method
[ 0.869110] i2c-core: driver [tsl2550] using legacy resume method
[ 0.875518] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.974487] No daughter card found
[ 0.978057] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.993255] Board name: A335BNLT
[ 0.996612] Board version: t
[ 0.996643] ue
[ 1.001373] The board is a AM335x Beaglebone Black.
[ 1.008483] tps65217 1-0024: TPS65217 ID 0xe version 1.2
[ 1.015991] print_constraints: DCDC1: 900 <--> 1800 mV at 1500 mV
[ 1.024414] print_constraints: DCDC2: 900 <--> 3300 mV at 1325 mV
[ 1.032775] print_constraints: DCDC3: 900 <--> 1500 mV at 1125 mV
[ 1.041168] print_constraints: LDO1: 1000 <--> 3300 mV at 1800 mV
[ 1.049682] print_constraints: LDO2: 900 <--> 3300 mV at 3300 mV
[ 1.058013] print_constraints: LDO3: 1800 <--> 3300 mV at 1800 mV
[ 1.066406] print_constraints: LDO4: 1800 <--> 3300 mV at 3300 mV
[ 1.073333] Maximum current provided by the USB port is 500mA which is not sufficient
[ 1.073333] when operating @OPP120 and OPPTURBO. The current requirement for some
[ 1.073333] use-cases using OPP100 might also exceed the maximum current that the
[ 1.073364] USB port can provide. Unless you are fully confident that the current
[ 1.073364] requirements for OPP100 use-case don't exceed the USB limits, switching
[ 1.073364] to AC power is recommended.
[ 1.117340] omap_hsmmc.0: alias fck already exists
[ 1.122741] omap_hsmmc.1: alias fck already exists
[ 1.128112] omap_i2c.3: alias fck already exists
[ 1.133300] omap_i2c omap_i2c.3: bus 3 rev2.4.0 at 100 kHz
[ 1.140777] registered am33xx_sr device
[ 1.146301] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.153320] omap2-nand driver initializing
[ 1.157775] OneNAND driver initializing
[ 1.162719] CAN device driver interface
[ 1.166748] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.214538] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.221008] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
[ 1.228149] davinci_mdio.0: probed
[ 1.231689] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720
[ 1.240509] usbcore: registered new interface driver zd1201
[ 1.246520] usbcore: registered new interface driver cdc_ether
[ 1.252716] usbcore: registered new interface driver cdc_eem
[ 1.258758] usbcore: registered new interface driver dm9601
[ 1.264617] cdc_ncm: 04-Aug-2011
[ 1.268096] usbcore: registered new interface driver cdc_ncm
[ 1.274017] Initializing USB Mass Storage driver...
[ 1.279296] usbcore: registered new interface driver usb-storage
[ 1.285583] USB Mass Storage support registered.
[ 1.290740] mousedev: PS/2 mouse device common for all mice
[ 1.297424] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[ 1.304626] i2c /dev entries driver
[ 1.308746] Linux video capture interface: v2.00
[ 1.313812] usbcore: registered new interface driver uvcvideo
[ 1.319854] USB Video Class driver (1.1.1)
[ 1.585296] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.592773] cpuidle: using governor ladder
[ 1.597442] cpuidle: using governor menu
[ 1.605010] omap4_aes_mod_init: loading AM33X AES driver
[ 1.610656] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[ 1.617309] omap4_aes_probe: probe() done
[ 1.621673] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[ 1.627807] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[ 1.644500] omap4_sham_probe: probe() done
[ 1.650665] usbcore: registered new interface driver usbhid
[ 1.656524] usbhid: USB HID core driver
[ 1.661132] usbcore: registered new interface driver snd-usb-audio
[ 1.668945] ALSA device list:
[ 1.672027] No soundcards found.
[ 1.675598] oprofile: hardware counters not available
[ 1.680877] oprofile: using timer interrupt.
[ 1.685363] nf_conntrack version 0.5.0 (8018 buckets, 32072 max)
[ 1.692077] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.697753] TCP cubic registered
[ 1.701141] NET: Registered protocol family 17
[ 1.705780] can: controller area network core (rev 20090105 abi 8)
[ 1.712310] NET: Registered protocol family 29
[ 1.716979] can: raw protocol (rev 20090105)
[ 1.721435] can: broadcast manager protocol (rev 20090105 t)
[ 1.727386] Registering the dns_resolver key type
[ 1.732360] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 1.740386] ThumbEE CPU extension supported.
[ 1.744903] mux: Failed to setup hwmod io irq -22
[ 1.750335] Power Management for AM33XX family
[ 1.755157] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 1.761840] Copied the M3 firmware to UMEM
[ 1.766204] Cortex M3 Firmware Version = 0x181
[ 1.771667] create_regulator: DCDC2: Failed to create debugfs directory
[ 1.779235] smartreflex smartreflex: am33xx_sr_probe: Driver initialized
[ 1.790130] clock: disabling unused clocks to save power
[ 1.803375] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 1.813964] mmc0: new high speed SDHC card at address 1234
[ 1.820251] Detected MACID=c8:a0:30:af:18:ae
[ 1.825836] cpsw: Detected MACID = c8:a0:30:af:18:b0
[ 1.831359] mmcblk0: mmc0:1234 SA08G 7.28 GiB
[ 1.837371] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:00:01 UTC (946684801)
[ 1.846649] mmcblk0: p1 p2
[ 1.854949] EXT3-fs (mmcblk0p2): recovery required on readonly filesystem
[ 1.862060] EXT3-fs (mmcblk0p2): write access will be enabled during recovery
[ 2.320800] mmc1: new high speed MMC card at address 0001
[ 2.327087] mmcblk1: mmc1:0001 MMC02G 1.78 GiB
[ 2.331909] mmcblk1boot0: mmc1:0001 MMC02G partition 1 1.00 MiB
[ 2.338195] mmcblk1boot1: mmc1:0001 MMC02G partition 2 1.00 MiB
[ 2.346618] mmcblk1: p1 p2
[ 2.351470] mmcblk1boot1: unknown partition table
[ 2.358032] mmcblk1boot0: unknown partition table
[ 8.019470] kjournald starting. Commit interval 5 seconds
[ 8.025299] EXT3-fs (mmcblk0p2): recovery complete
[ 8.883483] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[ 8.890716] VFS: Mounted root (ext3 filesystem) readonly on device 179:2.
[ 8.898132] Freeing init memory: 236K
INIT: version 2.88 booting
Starting udev
Error opening /dev/fb0: No such device
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
[ 11.945556] EXT3-fs (mmcblk0p2): using internal journal
ALSA: Restoring mixer settings...
Configuring network interfaces... /usr/sbin/alsactl: load_state:1686: No soundcards found...
[ 12.385650] net eth0: CPSW phy found : id is : 0x7c0f1
udhcpc (v1.20.2) started
Sending discover...
Sending discover...
Sending discover...
No lease, failing
done.
Tue Jun 25 23:08:00 UTC 2013
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
Stopping Bootlog daemon: bootlogd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyO0
Arago 2013.05 am335x-evm ttyO0
am335x-evm login: root
----------------------------------------------------------------------------------------------------
I think the M3 core has been successfully loaded, the red words above can query it.
But when type the suspend command as following:
root@am335x-evm:~# echo mem >/sys/power/state
[ 47.366333] PM: Syncing filesystems ... done.
[ 48.369110] Freezing user space processes ... (elapsed 0.01 seconds) done.
[ 48.388763] Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.
[ 48.408813] Suspending console(s) (use no_console_suspend to debug)
I can't wake up the board with power button. What should I do?