This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error in TI sitara Starter kit interfacing flash drive to Board (Error in Teraterm and Minicom)

root@am335x-evm:~#

[ 2936.826049] usb 1-1: new high-speed USB device number 5 using musb-hdrc
[ 2936.968078] usb 1-1: New USB device found, idVendor=058f, idProduct=6387
[ 2936.975067] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 2936.982543] usb 1-1: Product: Mass Storage Device
[ 2936.987457] usb 1-1: Manufacturer: JetFlash
[ 2936.991821] usb 1-1: SerialNumber: O3LQ1I1N
[ 2937.004638] scsi3 : usb-storage 1-1:1.0
[ 2938.007232] scsi 3:0:0:0: Direct-Access JetFlash TS512MJFV30 8.07 PQ: 0 ANSI: 2
[ 2938.026763] sd 3:0:0:0: [sda] 1004544 512-byte logical blocks: (514 MB/490 MiB)
[ 2938.046478] sd 3:0:0:0: [sda] Write Protect is off
[ 2938.058074] sd 3:0:0:0: [sda] No Caching mode page present
[ 2938.063812] sd 3:0:0:0: [sda] Assuming drive cache: write through
[ 2938.074523] sd 3:0:0:0: [sda] No Caching mode page present
[ 2938.080291] sd 3:0:0:0: [sda] Assuming drive cache: write through
[ 2938.219818] sda: sda1
[ 2938.226562] sd 3:0:0:0: [sda] No Caching mode page present
[ 2938.232269] sd 3:0:0:0: [sda] Assuming drive cache: write through
[ 2938.238647] sd 3:0:0:0: [sda] Attached SCSI removable disk
[ 2938.561004] FAT-fs (sda): invalid media value (0x00)
[ 2938.566253] FAT-fs (sda): Can't find a valid FAT filesystem

Which file system is support Because i formatted  the flash drive with ext,FAT,FAT32 but same error message it showing and procedure to mount to it