This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DMA operation of PCI-Express causes a problem when I install the ti81xxvo.ko

Other Parts Discussed in Thread: TVP5158

I'm testing the DMA transfer of PCI-Express.

In a state in which I have installed only the driver of the PCI first, DMA test app works fine.

Will fail to DMA test of PCIExpress Then, when you install the driver of the capture relationship.

I have installed the drivers in the following order, and the DMA test every time I install the drivers for each, the operation of the DMA will be abnormal when you installed the ti81xxvin.ko.

# install PCI-Express
insmod driver/altera_pci.ko debug=1
major=`grep altera_pci/proc/devices | cut -f1 -d" "`
mknod /dev/altera_pci c $major 0
chmod 666 /dev/altera_pci

# install PCI-Express
insmod driver/syslink.ko
./slaveloader_release startup VPSS-M3 dm816x_hdvpss_v4l2.xem3
insmod driver/vpss.ko
insmod driver/ti81xxfb.ko vram=0:30M,1:1M,2:10M
insmod driver/ti81xxvo.ko debug=1
insmod driver/tvp5158.ko
insmod driver/ti81xxvin.ko debug=1   <- It is abnormal here
insmod driver/ti81xxhdmi.ko

So what is happening?


<Normal test operation>
    DMA from 0x20000000 to 0xa6c00000(0xffd00000) size=0x00080000
    [Read Data]
             00 01 02 03 04 05 06 07  08 09 0A 0B 0C 0D 0E 0F
    20000000 00 00 02 00 04 00 06 00  08 00 0A 00 0C 00 0E 00
    
    [Before]
             00 01 02 03 04 05 06 07  08 09 0A 0B 0C 0D 0E 0F
    FFD00000 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00
    
    [After]
             00 01 02 03 04 05 06 07  08 09 0A 0B 0C 0D 0E 0F
    FFD00000 00 00 02 00 04 00 06 00  08 00 0A 00 0C 00 0E 00
    
    
<Abnormal test operation>

    DMA from 0x20000000 to 0xa6c00000(0xffd00000) size=0x00080000
    [Read Data]
             00 01 02 03 04 05 06 07  08 09 0A 0B 0C 0D 0E 0F
    20000000 00 00 02 00 04 00 06 00  08 00 0A 00 0C 00 0E 00
    
    [Before]
             00 01 02 03 04 05 06 07  08 09 0A 0B 0C 0D 0E 0F
    FFD00000 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00
    
    [After]
             00 01 02 03 04 05 06 07  08 09 0A 0B 0C 0D 0E 0F
    FFD00000 0F 00 02 0D 00 00 00 0F  00 0A 0A 0A 0A 0A 0A 0A