Other Parts Discussed in Thread: AM3352, LM3S1150, LM3S1512, LM3S1607, LM3S1601, LM3S1608, LM3S1626, LM3S1627, LM3S1751, LM3S1911, LM3S1918, LM3S1968, LM3S1960, LM3S2110, LM3S2139, LM3S2620, LM3S2608, LM3S2616, LM3S2739, LM3S2678, LM3S2911, LM3S2918, LM3S2950, LM3S2965, LM3S2948, LM3S300, LM3S301, LM3S315, LM3S310, LM3S308, LM3S3739, LM3S3634, LM3S3749, LM3S3748, LM3S5632, LM3S5732, LM3S5749, LM3S600, LM3S611, LM3S608, LM3S6100, LM3S615, LM3S617, LM3S618, LM3S6537, LM3S6432, LM3S6610, LM3S6911, LM3S6753, LM3S6730, LM3S6965, LM3S6938, LM3S6950, LM3S6918, LM3S811, LM3S801, LM3S800, LM3S808, LM3S818, LM3S817, LM3S8933, LM3S8970, LM3S8962, LM3S8938, SYSBIOS, LM3S8971, TMS320DM8168, TMS320DM8148, TM4C1290NCPDT, TM4C1290NCZAD, TM4C1294NCZAD, TM4C1294NCPDT, TM4C1292NCPDT, TM4C1292NCZAD, TM4C129CNCPDT, TM4C129CNCZAD, TM4C129DNCPDT, TM4C129DNCZAD, TM4C129ENCPDT, TM4C129ENCZAD, TM4E129BNCZAD, AM3359, AM3354, OMAP3503
I was trying to get some example code working to make sure my environment was setup correctly with CCS and the RTOS.
If I compile the non-RTOS hello example it compiles just fine however the SYS/BIOS hello world example errors out with "unsupported device". See output below.
I am sure this is a simple setup issue. I have the latest CCS, RTOS and AM335x starter kit installed. The goal is to build for a generic AM3352 configuration.
Thanks,
Aaron
**** Build of configuration Debug for project rtostest ****
"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all
'Building file: ../hello.cfg'
'Invoking: XDCtools'
"C:/ti/xdctools_3_25_00_48/xs" --xdcpath="C:/ti/bios_6_35_01_29/packages;C:/ti/tirtos_1_10_00_23/packages;C:/ti/tirtos_1_10_00_23/products/bios_6_35_01_29/packages;C:/ti/tirtos_1_10_00_23/products/ipc_1_25_03_15/packages;C:/ti/tirtos_1_10_00_23/products/ndk_2_22_03_20/packages;C:/ti/tirtos_1_10_00_23/products/uia_1_03_00_02/packages;C:/ti/ccsv5/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M3 -p ti.platforms.stellaris:AM3352 -r release -c "C:/ti/ccsv5/tools/compiler/arm_5.0.4" --compileOptions "-g --optimize_with_debug" "../hello.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring hello.xem3 from package/cfg/hello_pem3.cfg ...
The AM3352 device is not currently supported.
The following devices are supported in the ti.catalog.arm.cortexm3 catalog:
CortexM3 F28M35x LM3S101 LM3S102 LM3S1110
LM3S1133 LM3S1138 LM3S1150 LM3S1162 LM3S1165
LM3S1166 LM3S1332 LM3S1435 LM3S1439 LM3S1512
LM3S1538 LM3S1601 LM3S1607 LM3S1608 LM3S1620
LM3S1621 LM3S1625 LM3S1626 LM3S1627 LM3S1635
LM3S1636 LM3S1637 LM3S1651 LM3S1751 LM3S1776
LM3S1811 LM3S1816 LM3S1850 LM3S1911 LM3S1918
LM3S1937 LM3S1958 LM3S1960 LM3S1968 LM3S1969
LM3S1B21 LM3S1J11 LM3S1J16 LM3S1N11 LM3S1N16
LM3S1P51 LM3S1R21 LM3S1R26 LM3S1W16 LM3S1Z16
LM3S2016 LM3S2108 LM3S2110 LM3S2139 LM3S2276
LM3S2410 LM3S2412 LM3S2432 LM3S2533 LM3S2601
LM3S2608 LM3S2616 LM3S2620 LM3S2637 LM3S2651
LM3S2671 LM3S2678 LM3S2730 LM3S2739 LM3S2776
LM3S2793 LM3S2911 LM3S2918 LM3S2919 LM3S2939
LM3S2948 LM3S2950 LM3S2965 LM3S2B93 LM3S300
LM3S301 LM3S308 LM3S310 LM3S315 LM3S316
LM3S317 LM3S328 LM3S3634 LM3S3651 LM3S3739
LM3S3748 LM3S3749 LM3S3826 LM3S3J26 LM3S3N26
LM3S3W26 LM3S3Z26 LM3S5632 LM3S5651 LM3S5652
LM3S5656 LM3S5662 LM3S5732 LM3S5737 LM3S5739
LM3S5747 LM3S5749 LM3S5752 LM3S5762 LM3S5791
LM3S5951 LM3S5956 LM3S5B91 LM3S5K31 LM3S5K36
LM3S5P31 LM3S5P36 LM3S5P51 LM3S5P56 LM3S5R31
LM3S5R36 LM3S5T36 LM3S5Y36 LM3S600 LM3S601
LM3S608 LM3S610 LM3S6100 LM3S611 LM3S6110
LM3S612 LM3S613 LM3S615 LM3S617 LM3S618
LM3S628 LM3S6420 LM3S6422 LM3S6432 LM3S6537
LM3S6610 LM3S6611 LM3S6618 LM3S6633 LM3S6637
LM3S6730 LM3S6753 LM3S6816 LM3S6911 LM3S6916
LM3S6918 LM3S6938 LM3S6950 LM3S6952 LM3S6965
LM3S800 LM3S801 LM3S808 LM3S811 LM3S812
LM3S815 LM3S817 LM3S818 LM3S828 LM3S8530
LM3S8538 LM3S8630 LM3S8730 LM3S8733 LM3S8738
LM3S8930 LM3S8933 LM3S8938 LM3S8962 LM3S8970
js: "C:/ti/bios_6_35_01_29/packages/ti/sysbios/family/arm/Settings.xs", line 458: Error: Unsupported device!
"C:/ti/bios_6_35_01_29/packages/ti/sysbios/family/arm/Settings.xs", line 552
"C:/ti/bios_6_35_01_29/packages/ti/sysbios/family/Settings.xs", line 209
"C:/ti/bios_6_35_01_29/packages/ti/sysbios/family/Settings.xs", line 121
"C:/Users/aaron/workspace_v5_4/rtostest/hello.cfg", line 12
"./package/cfg/hello_pem3.cfg", line 180
LM3S8971 LM3S9781 LM3S9790 LM3S9792 LM3S9997
LM3S9B81 LM3S9B90 LM3S9B92 LM3S9B95 LM3S9B96
LM3S9L97 OMAP4430 OMAP5430 TMS320C6A8149 TMS320C6A8168
TMS320DM8148 TMS320DM8168 TMS320TI811X TMS320TI813X TMS320TI814X
TMS320TI816X
gmake.exe: *** [package/cfg/hello_pem3.xdl] Error 1
js: "C:/ti/xdctools_3_25_00_48/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake: Target `all' not remade because of errors.
**** Build Finished ****