This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unexpected HWI is triggered

Hello.

I want that HWI_15 would be triggered for the rising edge on GPIO55 on DM6437.

I set my TConf as following:

bios.HWI.instance("HWI_INT15").interruptSelectNumber = 75;
bios.HWI.instance("HWI_INT15").fxn = prog.extern("test_HWI_15");
bios.HWI.instance("HWI_INT15").useDispatcher = 1;
bios.HWI.instance("HWI_INT15").interruptMask = "all";

I configured GPIO55 as output, GPIO BINTEN with BANK 3, and SET_RIS_TRIG23 with GPIO55.

I also configured a periodic task which toggles the signal of GPIO55.

Tconf setup for the task is as below;

bios.PRD.create("PRD0");
bios.PRD.instance("PRD0").order = 1;
bios.PRD.instance("PRD0").comment = "1ms Periodic Timer";
bios.PRD.instance("PRD0").mode = "continuous";
bios.PRD.instance("PRD0").period = 980;
bios.PRD.instance("PRD0").fxn = prog.extern("test_PRD_clockPrd", "C");

When I run my code, HWI_INT4 was triggered but not HWI_INT15.

It seems that the interrupt is occured on a rising edge.

I also tried the interrupt selection number 2 according to SPRU403s, but I observed the same result.

bios.HWI.instance("HWI_INT15").interruptSelectNumber = 2;

I don't know why HWI_INT4 is triggered, instead of HWI_INT15.

Could someone help me?

Dongseung