This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467 video input port



We have a current product design where we are inputting 1080P60 (at 148.5MHz clock rate) into the video port of a DM6467 (729MHz grade).

We have made a relatively small number of these products, but all seem to work reliably over 0 - 45 degrees C temperature range. Do you have any feedback on whether we can expect this to be reliable over different batches of processors? Are there any other factors which would affect this performance (e.g. supply voltages, operating temperature)?