This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to enable two displays with different resolutions in dm814x

Hi, 

We are working on a DM8148 custom Board. We are connecting two displays 15" and 12" with resolutions 1280x800 and 800x600 respectively.

we have a qt application which is running on our board.

Currently we are using fb0 and graphics pipeline 0.

we want to get the application running on both the displays with different resolutions simultaneously on HDMI and DVO2. 

please help us in resolving this issue.