This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

look up nsp of 6614

hi.

   I want to add the ndk on 6614.but the nsp only support 6748. building is failed:

error info

undefined first referenced
symbol in file
--------- ----------------
NIMUDeviceTable D:\ti\ndk_2_21_01_38\packages\ti\ndk\stack\lib\stk6.ae66<nimu.oe66>

then I changed the nsp makefile.changed the out file is c66. the error (NIMUDeviceTable) is soloved.

but ccs did not find  EMAC_initialize()  ,EMAC_getConfig( UINT8 *pMacAddr),  EMAC_linkStatus( uint phy, uint linkStatus )

then I copy these functions in 6748's sample  to my project.

build ok!

but the network don't work .the hook function of netOpenHook() never start.

which step is error? thanks

  • TCI66xx devices are only supported through Field Applications Engineers (FAEs.)  These devices are not supported on the E2E forum.  Please contact your local FAE for support of TCI6614.  If you do not know who your local FAE is then please contact your local field sales and they would be happy to put you in contact with your local FAE.

    Best Regards,

    Chad