This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RDK4.0 SYSTEM: Attaching to [HOST] ...

Hi, sir

I'm using DVRRDK4.0, 2GB DDR, 512MB for Linux.

1) I set relative value in Rules.make,

  DDR_MEM := DDR_MEM_2048M
  LINUX_MEM := LINUX_MEM_512M

2) I run command : mkimage -A arm -O linux -T kernel -C none -a 0xc0008000 -e 0xc0008000 -n 'Linux-2.6.37' -d arch/arm/boot/zImage uImage        to modify the kernel for the new start address.

3) I set U-boot var, setenv bootargs ddr_mem=2048M mem=512M console=ttyO2,115200n8 ubi.mtd=4,2048 root=ubi0:rootfs rootwait=1 rootfstype=ubifs rw ip=129.1.10.140:129.1.9.231:129.1.9.1:255.255.0.0::eth0:off vram=20M notifyk.vpssm3_sva=0xBFB00000

4) tftp 0x81000000 129.1.9.231:uImage

bootm 0x81000000

5) entry .../rfs_816x/opt/dvr_rdk/ti816x

    ./init.sh       (passed)

    ./load.sh    (issue occured)

a) Info on terminal(telnet connection) , continuously

3162.Info_load.sh.pdf

b) Info on terminal(serial port connection)

6253.Info_load_serialport.pdf

I want to know how to fix this issue.

Appreciate for any guidance!