This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6747 MCASP0 problem with 96K sample/sec in slave mode.

Hi ,

I am using C6747 with OMAP L137 EVM board.

Test condition is

- OMAP L137, CCS 5.4

- EVMBOARD:  I2S(input) (slave) -> MCASP0 -> Loopback copy Task -> MCASP0 -> I2S (output) (slave)

I am successfully run 48Ksample per sec audio with these environment,but I increse sample rate to 96K sample per sec audio not work well.

I checked I2S input timing for 96Ksps signal, I believe it is no problem, but there is no I2S out signal.

I think 96K case also same as 48k register setting (AFSXCTL,ACLKXCTL, etc).

What should I have to do some more setting for 96Ksps compare with 48Ksps input ?

 

Doug

 

 

 

  • Hi Doug,

    Thanks for your post.

    It all depends on how you configure the McASP module as transmitter or receiver? Because there is clocking flexibility allows the McASP to receive and transmit at different rates and by this, McASP can receive data at 48Ksps but while transmit data, it has the flexibitlity to up-sample at 96Ksps or 192Ksps.

    Since your case is a loopback task, it would be better to operate both transmit and receive sections of McASP synchronously at same sample rate. Please refer Section 24.1.2 in the C6747 TRM as below:

    http://www.ti.com/lit/ug/spruh91b/spruh91b.pdf

    You can also refer the below E2E thread to get an idea of changing sample rates:

    http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/214513/766354.aspx#766354

    Also, you can refer the attached sample McASP loop back code from C6748 EVM Starterware package

    /**
     * \file  mcaspPlayBk.c
     *
     * \brief Sample application for McASP. This application loops back the input
     *        at LINE_IN of the EVM to the LINE_OUT of the EVM. 
     */
    
    /*
    * Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/ 
    *
    *  Redistribution and use in source and binary forms, with or without 
    *  modification, are permitted provided that the following conditions 
    *  are met:
    *
    *    Redistributions of source code must retain the above copyright 
    *    notice, this list of conditions and the following disclaimer.
    *
    *    Redistributions in binary form must reproduce the above copyright
    *    notice, this list of conditions and the following disclaimer in the 
    *    documentation and/or other materials provided with the   
    *    distribution.
    *
    *    Neither the name of Texas Instruments Incorporated nor the names of
    *    its contributors may be used to endorse or promote products derived
    *    from this software without specific prior written permission.
    *
    *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    */
    
    #include "edma_event.h" 
    #include "interrupt.h"
    #include "soc_C6748.h"
    #include "hw_syscfg0_C6748.h"
    #include "evmC6748.h"
    #include "codecif.h"
    #include "mcasp.h"
    #include "aic31.h"
    #include "edma.h"
    #include "psc.h"
    
    #include <string.h>
    
    /******************************************************************************
    **                      INTERNAL MACRO DEFINITIONS
    ******************************************************************************/
    /*
    ** Values which are configurable
    */
    /* Slot size to send/receive data */
    #define SLOT_SIZE                             (16u)
    
    /* Word size to send/receive data. Word size <= Slot size */
    #define WORD_SIZE                             (16u)
    
    /* Sampling Rate which will be used by both transmit and receive sections */
    #define SAMPLING_RATE                         (48000u)
    
    /* Number of channels, L & R */
    #define NUM_I2S_CHANNELS                      (2u) 
    
    /* Number of samples to be used per audio buffer */
    #define NUM_SAMPLES_PER_AUDIO_BUF             (2000u)
    
    /* Number of buffers used per tx/rx */
    #define NUM_BUF                               (3u)
    
    /* Number of linked parameter set used per tx/rx */
    #define NUM_PAR                               (2u)
    
    /* Specify where the parameter set starting is */
    #define PAR_ID_START                          (40u)
    
    /* Number of samples in loop buffer */
    #define NUM_SAMPLES_LOOP_BUF                  (10u)
    
    /* AIC3106 codec address */
    #define I2C_SLAVE_CODEC_AIC31                 (0x18u) 
    
    /* Interrupt channels to map in AINTC */
    #define INT_CHANNEL_I2C                       (2u)
    #define INT_CHANNEL_MCASP                     (2u)
    #define INT_CHANNEL_EDMACC                    (2u)
    
    /* McASP Serializer for Receive */
    #define MCASP_XSER_RX                         (12u)
    
    /* McASP Serializer for Transmit */
    #define MCASP_XSER_TX                         (11u)
    
    /*
    ** Below Macros are calculated based on the above inputs
    */
    #define NUM_TX_SERIALIZERS                    ((NUM_I2S_CHANNELS >> 1) \
                                                   + (NUM_I2S_CHANNELS & 0x01))
    #define NUM_RX_SERIALIZERS                    ((NUM_I2S_CHANNELS >> 1) \
                                                   + (NUM_I2S_CHANNELS & 0x01))
    #define I2S_SLOTS                             ((1 << NUM_I2S_CHANNELS) - 1)
    
    #define BYTES_PER_SAMPLE                      ((WORD_SIZE >> 3) \
                                                   * NUM_I2S_CHANNELS)
    
    #define AUDIO_BUF_SIZE                        (NUM_SAMPLES_PER_AUDIO_BUF \
                                                   * BYTES_PER_SAMPLE)
    
    #define TX_DMA_INT_ENABLE                     (EDMA3CC_OPT_TCC_SET(1) | (1 \
                                                   << EDMA3CC_OPT_TCINTEN_SHIFT))
    #define RX_DMA_INT_ENABLE                     (EDMA3CC_OPT_TCC_SET(0) | (1 \
                                                   << EDMA3CC_OPT_TCINTEN_SHIFT))
    
    #define PAR_RX_START                          (PAR_ID_START)
    #define PAR_TX_START                          (PAR_RX_START + NUM_PAR)
    
    /*
    ** Definitions which are not configurable 
    */
    #define SIZE_PARAMSET                         (32u)
    #define OPT_FIFO_WIDTH                        (0x02 << 8u)
    
    /******************************************************************************
    **                      INTERNAL FUNCTION PROTOTYPES
    ******************************************************************************/
    static void McASPErrorIsr(void);
    static void McASPErrorIntSetup(void);
    static void AIC31I2SConfigure(void);
    static void McASPI2SConfigure(void);
    static void McASPTxDMAComplHandler(void);
    static void McASPRxDMAComplHandler(void);
    static void EDMA3CCComplIsr(void);
    static void I2SDataTxRxActivate(void);
    static void I2SDMAParamInit(void);
    static void ParamTxLoopJobSet(unsigned short parId);
    static void BufferTxDMAActivate(unsigned int txBuf, unsigned short numSamples,
                                    unsigned short parToUpdate, 
                                    unsigned short linkAddr);
    static void BufferRxDMAActivate(unsigned int rxBuf, unsigned short parId,
                                    unsigned short parLink);
    
    /******************************************************************************
    **                      INTERNAL VARIABLE DEFINITIONS
    ******************************************************************************/
    static unsigned char loopBuf[NUM_SAMPLES_LOOP_BUF * BYTES_PER_SAMPLE] = {0};
    
    /*
    ** Transmit buffers. If any new buffer is to be added, define it here and 
    ** update the NUM_BUF.
    */
    static unsigned char txBuf0[AUDIO_BUF_SIZE];
    static unsigned char txBuf1[AUDIO_BUF_SIZE];
    static unsigned char txBuf2[AUDIO_BUF_SIZE];
    
    /*
    ** Receive buffers. If any new buffer is to be added, define it here and 
    ** update the NUM_BUF.
    */
    static unsigned char rxBuf0[AUDIO_BUF_SIZE];
    static unsigned char rxBuf1[AUDIO_BUF_SIZE];
    static unsigned char rxBuf2[AUDIO_BUF_SIZE];
    
    /*
    ** Next buffer to receive data. The data will be received in this buffer.
    */
    static volatile unsigned int nxtBufToRcv = 0;
    
    /*
    ** The RX buffer which filled latest.
    */
    static volatile unsigned int lastFullRxBuf = 0;
    
    /*
    ** The offset of the paRAM ID, from the starting of the paRAM set.
    */
    static volatile unsigned short parOffRcvd = 0;
    
    /*
    ** The offset of the paRAM ID sent, from starting of the paRAM set.
    */
    static volatile unsigned short parOffSent = 0;
    
    /*
    ** The offset of the paRAM ID to be sent next, from starting of the paRAM set. 
    */
    static volatile unsigned short parOffTxToSend = 0;
    
    /*
    ** The transmit buffer which was sent last.
    */
    static volatile unsigned int lastSentTxBuf = NUM_BUF - 1;
    
    /******************************************************************************
    **                      INTERNAL CONSTATNT DEFINITIONS
    ******************************************************************************/
    /* Array of receive buffer pointers */
    static unsigned int const rxBufPtr[NUM_BUF] =
           { 
               (unsigned int) rxBuf0,
               (unsigned int) rxBuf1,
               (unsigned int) rxBuf2
           };
    
    /* Array of transmit buffer pointers */
    static unsigned int const txBufPtr[NUM_BUF] =
           { 
               (unsigned int) txBuf0,
               (unsigned int) txBuf1,
               (unsigned int) txBuf2
           };
    
    /*
    ** Default paRAM for Transmit section. This will be transmitting from 
    ** a loop buffer.
    */
    static struct EDMA3CCPaRAMEntry const txDefaultPar = 
           {
               (unsigned int)(EDMA3CC_OPT_DAM  | (0x02 << 8u)), /* Opt field */
               (unsigned int)loopBuf, /* source address */
               (unsigned short)(BYTES_PER_SAMPLE), /* aCnt */
               (unsigned short)(NUM_SAMPLES_LOOP_BUF), /* bCnt */ 
               (unsigned int) SOC_MCASP_0_DATA_REGS, /* dest address */
               (short) (BYTES_PER_SAMPLE), /* source bIdx */
               (short)(0), /* dest bIdx */
               (unsigned short)(PAR_TX_START * SIZE_PARAMSET), /* link address */
               (unsigned short)(0), /* bCnt reload value */
               (short)(0), /* source cIdx */
               (short)(0), /* dest cIdx */
               (unsigned short)1 /* cCnt */
           };
    
    /*
    ** Default paRAM for Receive section.  
    */
    static struct EDMA3CCPaRAMEntry const rxDefaultPar =
           {
               (unsigned int)(EDMA3CC_OPT_SAM  | (0x02 << 8u)), /* Opt field */
               (unsigned int)SOC_MCASP_0_DATA_REGS, /* source address */
               (unsigned short)(BYTES_PER_SAMPLE), /* aCnt */
               (unsigned short)(1), /* bCnt */
               (unsigned int)rxBuf0, /* dest address */
               (short) (0), /* source bIdx */
               (short)(BYTES_PER_SAMPLE), /* dest bIdx */
               (unsigned short)(PAR_RX_START * SIZE_PARAMSET), /* link address */
               (unsigned short)(0), /* bCnt reload value */
               (short)(0), /* source cIdx */
               (short)(0), /* dest cIdx */
               (unsigned short)1 /* cCnt */
           };
    
    /******************************************************************************
    **                          FUNCTION DEFINITIONS
    ******************************************************************************/
    /*
    ** Assigns loop job for a parameter set
    */
    static void ParamTxLoopJobSet(unsigned short parId)
    {
        EDMA3CCPaRAMEntry paramSet;
        
        memcpy(&paramSet, &txDefaultPar, SIZE_PARAMSET - 2);
      
        /* link the paRAM to itself */
        paramSet.linkAddr = parId * SIZE_PARAMSET;
    
        EDMA3SetPaRAM(SOC_EDMA30CC_0_REGS, parId, &paramSet);
    }
    
    /*
    ** Initializes the DMA parameters.
    ** The RX basic paRAM set(channel) is 0 and TX basic paRAM set (channel) is 1.
    **
    ** The RX paRAM set 0 will be initialized to receive data in the rx buffer 0.
    ** The transfer completion interrupt will not be enabled for paRAM set 0;
    ** paRAM set 0 will be linked to linked paRAM set starting (PAR_RX_START) of RX.
    ** and further reception only happens via linked paRAM set. 
    ** For example, if the PAR_RX_START value is 40, and the number of paRAMS is 2, 
    ** reception paRAM set linking will be initialized as 0-->40-->41-->40
    **
    ** The TX paRAM sets will be initialized to transmit from the loop buffer.
    ** The size of the loop buffer can be configured.   
    ** The transfer completion interrupt will not be enabled for paRAM set 1;
    ** paRAM set 1 will be linked to linked paRAM set starting (PAR_TX_START) of TX.
    ** All other paRAM sets will be linked to itself.
    ** and further transmission only happens via linked paRAM set.
    ** For example, if the PAR_RX_START value is 42, and the number of paRAMS is 2, 
    ** So transmission paRAM set linking will be initialized as 1-->42-->42, 43->43. 
    */
    static void I2SDMAParamInit(void)
    {
        EDMA3CCPaRAMEntry paramSet;
        int idx; 
     
        /* Initialize the 0th paRAM set for receive */ 
        memcpy(&paramSet, &rxDefaultPar, SIZE_PARAMSET - 2);
    
        EDMA3SetPaRAM(SOC_EDMA30CC_0_REGS, EDMA3_CHA_MCASP0_RX, &paramSet);
    
        /* further paramsets, enable interrupt */
        paramSet.opt |= RX_DMA_INT_ENABLE; 
     
        for(idx = 0 ; idx < NUM_PAR; idx++)
        {
            paramSet.destAddr = rxBufPtr[idx];
    
            paramSet.linkAddr = (PAR_RX_START + ((idx + 1) % NUM_PAR)) 
                                 * (SIZE_PARAMSET);        
    
            paramSet.bCnt =  NUM_SAMPLES_PER_AUDIO_BUF;
    
            /* 
            ** for the first linked paRAM set, start receiving the second
            ** sample only since the first sample is already received in
            ** rx buffer 0 itself.
            */
            if( 0 == idx)
            {
                paramSet.destAddr += BYTES_PER_SAMPLE;
                paramSet.bCnt -= BYTES_PER_SAMPLE;
            }
    
            EDMA3SetPaRAM(SOC_EDMA30CC_0_REGS, (PAR_RX_START + idx), &paramSet);
        } 
    
        /* Initialize the required variables for reception */
        nxtBufToRcv = idx % NUM_BUF;
        lastFullRxBuf = NUM_BUF - 1;
        parOffRcvd = 0;
    
        /* Initialize the 1st paRAM set for transmit */ 
        memcpy(&paramSet, &txDefaultPar, SIZE_PARAMSET);
    
        EDMA3SetPaRAM(SOC_EDMA30CC_0_REGS, EDMA3_CHA_MCASP0_TX, &paramSet);
    
        /* rest of the params, enable loop job */
        for(idx = 0 ; idx < NUM_PAR; idx++)
        {
            ParamTxLoopJobSet(PAR_TX_START + idx);
        }
     
        /* Initialize the variables for transmit */
        parOffSent = 0;
        lastSentTxBuf = NUM_BUF - 1; 
    }
    
    /*
    ** Function to configure the codec for I2S mode
    */
    static void AIC31I2SConfigure(void)
    {
        volatile unsigned int delay = 0xFFF;
    
        AIC31Reset(SOC_I2C_0_REGS);
        while(delay--);
    
        /* Configure the data format and sampling rate */
        AIC31DataConfig(SOC_I2C_0_REGS, AIC31_DATATYPE_I2S, SLOT_SIZE, 0);
        AIC31SampleRateConfig(SOC_I2C_0_REGS, AIC31_MODE_BOTH, SAMPLING_RATE);
    
        /* Initialize both ADC and DAC */
        AIC31ADCInit(SOC_I2C_0_REGS);
        AIC31DACInit(SOC_I2C_0_REGS);
    }
    
    /*
    ** Configures the McASP Transmit Section in I2S mode.
    */
    static void McASPI2SConfigure(void)
    {
        McASPRxReset(SOC_MCASP_0_CTRL_REGS);
        McASPTxReset(SOC_MCASP_0_CTRL_REGS);
    
        /* Enable the FIFOs for DMA transfer */
        McASPReadFifoEnable(SOC_MCASP_0_FIFO_REGS, 1, 1);
        McASPWriteFifoEnable(SOC_MCASP_0_FIFO_REGS, 1, 1);
    
        /* Set I2S format in the transmitter/receiver format units */
        McASPRxFmtI2SSet(SOC_MCASP_0_CTRL_REGS, WORD_SIZE, SLOT_SIZE,
                         MCASP_RX_MODE_DMA);
        McASPTxFmtI2SSet(SOC_MCASP_0_CTRL_REGS, WORD_SIZE, SLOT_SIZE,
                         MCASP_TX_MODE_DMA);
    
        /* Configure the frame sync. I2S shall work in TDM format with 2 slots */
        McASPRxFrameSyncCfg(SOC_MCASP_0_CTRL_REGS, 2, MCASP_RX_FS_WIDTH_WORD, 
                            MCASP_RX_FS_EXT_BEGIN_ON_RIS_EDGE);
        McASPTxFrameSyncCfg(SOC_MCASP_0_CTRL_REGS, 2, MCASP_TX_FS_WIDTH_WORD, 
                            MCASP_TX_FS_EXT_BEGIN_ON_RIS_EDGE);
    
        /* configure the clock for receiver */
        McASPRxClkCfg(SOC_MCASP_0_CTRL_REGS, MCASP_RX_CLK_EXTERNAL, 0, 0);
        McASPRxClkPolaritySet(SOC_MCASP_0_CTRL_REGS, MCASP_RX_CLK_POL_RIS_EDGE); 
        McASPRxClkCheckConfig(SOC_MCASP_0_CTRL_REGS, MCASP_RX_CLKCHCK_DIV32,
                              0x00, 0xFF);
    
        /* configure the clock for transmitter */
        McASPTxClkCfg(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLK_EXTERNAL, 0, 0);
        McASPTxClkPolaritySet(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLK_POL_FALL_EDGE); 
        McASPTxClkCheckConfig(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLKCHCK_DIV32,
                              0x00, 0xFF);
     
        /* Enable synchronization of RX and TX sections  */  
        McASPTxRxClkSyncEnable(SOC_MCASP_0_CTRL_REGS);
    
        /* Enable the transmitter/receiver slots. I2S uses 2 slots */
        McASPRxTimeSlotSet(SOC_MCASP_0_CTRL_REGS, I2S_SLOTS);
        McASPTxTimeSlotSet(SOC_MCASP_0_CTRL_REGS, I2S_SLOTS);
    
        /*
        ** Set the serializers, Currently only one serializer is set as
        ** transmitter and one serializer as receiver.
        */
        McASPSerializerRxSet(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_RX);
        McASPSerializerTxSet(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_TX);
    
        /*
        ** Configure the McASP pins 
        ** Input - Frame Sync, Clock and Serializer Rx
        ** Output - Serializer Tx is connected to the input of the codec 
        */
        McASPPinMcASPSet(SOC_MCASP_0_CTRL_REGS, 0xFFFFFFFF);
        McASPPinDirOutputSet(SOC_MCASP_0_CTRL_REGS, MCASP_PIN_AXR(MCASP_XSER_TX));
        McASPPinDirInputSet(SOC_MCASP_0_CTRL_REGS, MCASP_PIN_AFSX 
                                                   | MCASP_PIN_ACLKX
                                                   | MCASP_PIN_AFSR
                                                   | MCASP_PIN_ACLKR
                                                   | MCASP_PIN_AXR(MCASP_XSER_RX));
    
        /* Enable error interrupts for McASP */
        McASPTxIntEnable(SOC_MCASP_0_CTRL_REGS, MCASP_TX_DMAERROR 
                                                | MCASP_TX_CLKFAIL 
                                                | MCASP_TX_SYNCERROR
                                                | MCASP_TX_UNDERRUN);
    
        McASPRxIntEnable(SOC_MCASP_0_CTRL_REGS, MCASP_RX_DMAERROR 
                                                | MCASP_RX_CLKFAIL
                                                | MCASP_RX_SYNCERROR 
                                                | MCASP_RX_OVERRUN);
    }
    
    /*
    ** Sets up the interrupts for EDMA in AINTC
    */
    static void EDMA3IntSetup(void)
    {
    #ifdef _TMS320C6X
    	IntRegister(C674X_MASK_INT5, EDMA3CCComplIsr);
    	IntEventMap(C674X_MASK_INT5, SYS_INT_EDMA3_0_CC0_INT1);
    	IntEnable(C674X_MASK_INT5);
    #else
        IntRegister(SYS_INT_CCINT0, EDMA3CCComplIsr);
        IntChannelSet(SYS_INT_CCINT0, INT_CHANNEL_EDMACC); 
        IntSystemEnable(SYS_INT_CCINT0);
    #endif
    }
    
    /*
    ** Sets up the error interrupts for McASP in AINTC
    */
    static void McASPErrorIntSetup(void)
    {
    #ifdef _TMS320C6X
    	IntRegister(C674X_MASK_INT6, McASPErrorIsr);
    	IntEventMap(C674X_MASK_INT6, SYS_INT_MCASP0_INT);
    	IntEnable(C674X_MASK_INT6);
    #else
        /* Register the error ISR for McASP */
        IntRegister(SYS_INT_MCASPINT, McASPErrorIsr);
    
        IntChannelSet(SYS_INT_MCASPINT, INT_CHANNEL_MCASP);
        IntSystemEnable(SYS_INT_MCASPINT);
    #endif
    }
    
    /*
    ** Activates the data transmission/reception
    ** The DMA parameters shall be ready before calling this function.
    */
    static void I2SDataTxRxActivate(void)
    {
        /* Start the clocks */
        McASPRxClkStart(SOC_MCASP_0_CTRL_REGS, MCASP_RX_CLK_EXTERNAL);
        McASPTxClkStart(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLK_EXTERNAL);
    
        /* Enable EDMA for the transfer */
        EDMA3EnableTransfer(SOC_EDMA30CC_0_REGS, EDMA3_CHA_MCASP0_RX,
                            EDMA3_TRIG_MODE_EVENT);
        EDMA3EnableTransfer(SOC_EDMA30CC_0_REGS, 
                            EDMA3_CHA_MCASP0_TX, EDMA3_TRIG_MODE_EVENT);
    
        /* Activate the  serializers */
        McASPRxSerActivate(SOC_MCASP_0_CTRL_REGS);
        McASPTxSerActivate(SOC_MCASP_0_CTRL_REGS);
    
        /* make sure that the XDATA bit is cleared to zero */
        while(McASPTxStatusGet(SOC_MCASP_0_CTRL_REGS) & MCASP_TX_STAT_DATAREADY);
    
        /* Activate the state machines */
        McASPRxEnable(SOC_MCASP_0_CTRL_REGS);
        McASPTxEnable(SOC_MCASP_0_CTRL_REGS);
    }
    
    /*
    ** Activates the DMA transfer for a parameterset from the given buffer.
    */
    void BufferTxDMAActivate(unsigned int txBuf, unsigned short numSamples,
                             unsigned short parId, unsigned short linkPar)
    {
        EDMA3CCPaRAMEntry paramSet;
    
        /* Copy the default paramset */
        memcpy(&paramSet, &txDefaultPar, SIZE_PARAMSET - 2);
        
        /* Enable completion interrupt */
        paramSet.opt |= TX_DMA_INT_ENABLE;
        paramSet.srcAddr =  txBufPtr[txBuf];
        paramSet.linkAddr = linkPar * SIZE_PARAMSET;  
        paramSet.bCnt = numSamples;
    
        EDMA3SetPaRAM(SOC_EDMA30CC_0_REGS, parId, &paramSet);
    }
    
    /*
    ** The main function. Application starts here.
    */
    int main(void)
    {
        unsigned short parToSend;
        unsigned short parToLink;
    
        /* Set up pin mux for I2C module 0 */
        I2CPinMuxSetup(0);
        McASPPinMuxSetup();
    
        /* Power up the McASP module */
        PSCModuleControl(SOC_PSC_1_REGS, HW_PSC_MCASP0, PSC_POWERDOMAIN_ALWAYS_ON,
    		     PSC_MDCTL_NEXT_ENABLE);
    
        /* Power up EDMA3CC_0 and EDMA3TC_0 */
        PSCModuleControl(SOC_PSC_0_REGS, HW_PSC_CC0, PSC_POWERDOMAIN_ALWAYS_ON,
    		     PSC_MDCTL_NEXT_ENABLE);
        PSCModuleControl(SOC_PSC_0_REGS, HW_PSC_TC0, PSC_POWERDOMAIN_ALWAYS_ON,
    		     PSC_MDCTL_NEXT_ENABLE);
    
    #ifdef _TMS320C6X
        // Initialize the DSP interrupt controller
        IntDSPINTCInit();
    #else
        /* Initialize the ARM Interrupt Controller.*/
        IntAINTCInit();
    #endif
    
        /* Initialize the I2C 0 interface for the codec AIC31 */
        I2CCodecIfInit(SOC_I2C_0_REGS, INT_CHANNEL_I2C, I2C_SLAVE_CODEC_AIC31);
    
        EDMA3Init(SOC_EDMA30CC_0_REGS, 0);
        EDMA3IntSetup(); 
    
        McASPErrorIntSetup();
      
    #ifdef _TMS320C6X
        IntGlobalEnable();
    #else
        /* Enable the interrupts generation at global level */ 
        IntMasterIRQEnable();
        IntGlobalEnable();
        IntIRQEnable();
    #endif
    
        /*
        ** Request EDMA channels. Channel 0 is used for reception and
        ** Channel 1 is used for transmission
        */
        EDMA3RequestChannel(SOC_EDMA30CC_0_REGS, EDMA3_CHANNEL_TYPE_DMA,
                            EDMA3_CHA_MCASP0_TX, EDMA3_CHA_MCASP0_TX, 0);
        EDMA3RequestChannel(SOC_EDMA30CC_0_REGS, EDMA3_CHANNEL_TYPE_DMA,
                            EDMA3_CHA_MCASP0_RX, EDMA3_CHA_MCASP0_RX, 0);
    
        /* Initialize the DMA parameters */
        I2SDMAParamInit();
    
        /* Configure the Codec for I2S mode */
        AIC31I2SConfigure();
    
        /* Configure the McASP for I2S */
        McASPI2SConfigure();
      
        /* Activate the audio transmission and reception */ 
        I2SDataTxRxActivate();
       
        /*
        ** Looop forever. if a new buffer is received, the lastFullRxBuf will be 
        ** updated in the rx completion ISR. if it is not the lastSentTxBuf, 
        ** buffer is to be sent. This has to be mapped to proper paRAM set.
        */
        while(1)
        {
            if(lastFullRxBuf != lastSentTxBuf)
            {  
                /*
                ** Start the transmission from the link paramset. The param set 
                ** 1 will be linked to param set at PAR_TX_START. So do not 
                ** update paRAM set1.
                */ 
                parToSend =  PAR_TX_START + (parOffTxToSend % NUM_PAR);
                parOffTxToSend = (parOffTxToSend + 1) % NUM_PAR;
                parToLink  = PAR_TX_START + parOffTxToSend; 
     
                lastSentTxBuf = (lastSentTxBuf + 1) % NUM_BUF;
    
                /* Copy the buffer */
                memcpy((void *)txBufPtr[lastSentTxBuf],
                       (void *)rxBufPtr[lastFullRxBuf],
                       AUDIO_BUF_SIZE);
    
                /*
                ** Send the buffer by setting the DMA params accordingly.
                ** Here the buffer to send and number of samples are passed as
                ** parameters. This is important, if only transmit section 
                ** is to be used.
                */
                BufferTxDMAActivate(lastSentTxBuf, NUM_SAMPLES_PER_AUDIO_BUF,
                                    (unsigned short)parToSend,
                                    (unsigned short)parToLink);
            }
        }
    }  
    
    /*
    ** Activates the DMA transfer for a parameter set from the given buffer.
    */
    static void BufferRxDMAActivate(unsigned int rxBuf, unsigned short parId,
                                    unsigned short parLink)
    {
        EDMA3CCPaRAMEntry paramSet;
    
        /* Copy the default paramset */
        memcpy(&paramSet, &rxDefaultPar, SIZE_PARAMSET - 2);
    
        /* Enable completion interrupt */
        paramSet.opt |= RX_DMA_INT_ENABLE;
        paramSet.destAddr =  rxBufPtr[rxBuf];
        paramSet.bCnt =  NUM_SAMPLES_PER_AUDIO_BUF;
        paramSet.linkAddr = parLink * SIZE_PARAMSET ;
    
        EDMA3SetPaRAM(SOC_EDMA30CC_0_REGS, parId, &paramSet);
    }
    
    /*
    ** This function will be called once receive DMA is completed
    */
    static void McASPRxDMAComplHandler(void)
    {
        unsigned short nxtParToUpdate;
    
        /*
        ** Update lastFullRxBuf to indicate a new buffer reception
        ** is completed.
        */
        lastFullRxBuf = (lastFullRxBuf + 1) % NUM_BUF;
        nxtParToUpdate =  PAR_RX_START + parOffRcvd;  
        parOffRcvd = (parOffRcvd + 1) % NUM_PAR;
     
        /*
        ** Update the DMA parameters for the received buffer to receive
        ** further data in proper buffer
        */
        BufferRxDMAActivate(nxtBufToRcv, nxtParToUpdate,
                            PAR_RX_START + parOffRcvd);
        
        /* update the next buffer to receive data */ 
        nxtBufToRcv = (nxtBufToRcv + 1) % NUM_BUF;
    }
    
    /*
    ** This function will be called once transmit DMA is completed
    */
    static void McASPTxDMAComplHandler(void)
    {
        ParamTxLoopJobSet((unsigned short)(PAR_TX_START + parOffSent));
    
        parOffSent = (parOffSent + 1) % NUM_PAR;
    }
    
    /*
    ** EDMA transfer completion ISR
    */
    static void EDMA3CCComplIsr(void) 
    { 
    #ifdef _TMS320C6X
    	IntEventClear(SYS_INT_EDMA3_0_CC0_INT1);
    #else
        IntSystemStatusClear(SYS_INT_CCINT0);
    #endif
    
        /* Check if receive DMA completed */
        if(EDMA3GetIntrStatus(SOC_EDMA30CC_0_REGS) & (1 << EDMA3_CHA_MCASP0_RX)) 
        { 
            /* Clear the interrupt status for the 0th channel */
            EDMA3ClrIntr(SOC_EDMA30CC_0_REGS, EDMA3_CHA_MCASP0_RX); 
            McASPRxDMAComplHandler();
        }
        
        /* Check if transmit DMA completed */
        if(EDMA3GetIntrStatus(SOC_EDMA30CC_0_REGS) & (1 << EDMA3_CHA_MCASP0_TX)) 
        { 
            /* Clear the interrupt status for the first channel */
            EDMA3ClrIntr(SOC_EDMA30CC_0_REGS, EDMA3_CHA_MCASP0_TX); 
            McASPTxDMAComplHandler();
        }
    }
    
    /*
    ** Error ISR for McASP
    */
    static void McASPErrorIsr(void)
    {
    #ifdef _TMS320C6X
    	IntEventClear(SYS_INT_MCASP0_INT);
    #else
        IntSystemStatusClear(SYS_INT_MCASPINT);
    #endif
    
        ; /* Perform any error handling here.*/
    }
    
    /***************************** End Of File ***********************************/
    

    Thanks & regards,

    Sivaraj K

    ---------------------------------------------------------------------------------
    Please click the
    Verify Answer button on this post if it answers your question.
    ---------------------------------------------------------------------------------

  • Hi ,

    Thank you for your kind answer.

    After change sample rate 48k to 96k, ISR routine is not work,

    I think internally interrupt is not work, basically It is work ok in 48k, that's why BIOS interrupt setting is no problem.

    This is my McASP setting.

    ---------

            mcasp0 = &MCASP_MODULE_0;
            /* ---------------------------------------------------------------- *
             *                                                                  *
             *  McASP0 is in Slave mode.                                       *
             *      BCLK & WCLK come from McASP0                                *
             *      DIN is used by write32/write32                              *
             *      DOUT is usec by read32/read32                               *
             *                                                                  *
             * ---------------------------------------------------------------- */
            mcasp0->regs->GBLCTL  = 0;       // Reset
            mcasp0->regs->RGBLCTL = 0;       // Reset RX
            mcasp0->regs->XGBLCTL = 0;       // Reset TX
            mcasp0->regs->PWRDEMU = 1;       // Free-running

              /* RX */
            mcasp0->regs->RMASK      = 0xffffffff; // No padding used
            mcasp0->regs->RFMT       = 0x000180F8; // MSB 32bit, 1-delay, no pad, CFGBus, No ROR
            mcasp0->regs->AFSRCTL    = 0x00000110; // 2TDM, 1bit Rising, INTERNAL FS, word
            mcasp0->regs->ACLKRCTL   = 0x0000008F; // Rising EXTERNAL CLK,(from tx side)
            mcasp0->regs->AHCLKRCTL  = 0x00000000; // INT CLK (from tx side)
            mcasp0->regs->RTDM       = 0x00000003; // Slots 0,1
            mcasp0->regs->RINTCTL    = 0x00000000; // Not used
            mcasp0->regs->RCLKCHK    = 0x00FF0008; // 255-MAX 0-MIN, div-by-256

            /* TX */
            mcasp0->regs->XMASK      = 0xffffffff; // No padding used
            mcasp0->regs->XFMT       = 0x000180F8; // MSB 16bit, 1-delay, no pad, CFGBus, No ROR
            mcasp0->regs->AFSXCTL    = 0x00000110; // 2TDM, 1bit Rising edge EXTERNAL FS, word
            mcasp0->regs->ACLKXCTL   = 0x0000008F; // ASYNC, Failing, EXTERNAL CLK, div-by-16
            mcasp0->regs->AHCLKXCTL  = 0x00000000; // EXT CLK
            mcasp0->regs->XTDM       = 0x00000003; // Slots 0,1
            mcasp0->regs->XINTCTL    = 0x00000000; // Not used
            mcasp0->regs->XCLKCHK    = 0x00FF0008; // 255-MAX 0-MIN, div-by-256

            mcasp0->regs->SRCTL5     = 0x000D;     // MCASP0.AXR0[5] --> DIN
            mcasp0->regs->SRCTL0     = 0x000E;     // MCASP0.AXR0[0] <-- DOUT
            mcasp0->regs->PFUNC      = 0;          // All MCASPs
            mcasp0->regs->PDIR       = 0x40000020; // All inputs except AXR0[5], AHCLKX0

            mcasp0->regs->DITCTL     = 0x00000000; // Not used
            mcasp0->regs->DLBCTL     = 0x00000000; // Not used
            mcasp0->regs->AMUTE      = 0x00000000; // Not used