This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MPU Registers discrepance C6678

I can not correctly identify the base address for the the mpu registers.

In the C6678 Datasheet Table 7-51 MPU Memory Regions

Memory Protection                    Start Address   End Address
MPU0    Main CFG TeraNet     0x01D00000    0x026207FF
MPU1    QM_SS DATA PORT  0x34000000     0x340BFFFF
MPU2    QM_SS CFG PORT    0x02A00000     0x02ABFFFF
MPU3    Semaphore                 0x02640000     0x026407FF

But the address of these registers do not correspond to those for the mpu in the memory map

0x02360000 - 0x023603FF   Memory Protection Unit (MPU) 0
0x02368000 - 0x023683FF   Memory Protection Unit (MPU) 1
0x02370000 - 0x023703FF   Memory Protection Unit (MPU) 2
0x02378000 - 0x023783FF   Memory Protection Unit (MPU) 3

Am I misinterpreting one of the tables?