This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[SMJ320C6701] GPO port

Other Parts Discussed in Thread: SMJ320C6701

Hi,

When I checked SMJ320C6701 datasheet, it has TOUT0(M18) & TOUT1(G2) can be used GPO port.

Does it have additional GPO port in SMJ320C6701? I can not find GPIO port in datasheet.

Thanks.

Robin

  • Hi Robin,

    Thanks for your post.

    Yes, you are right, Timer0 (TOUT0) and Timer1 (TOUT1) can be configured as general purpose outputs and as you said, there is no dedicated GPIO peripheral in SMJ320C6701 device and it cannot be used as software configurable GPIO pins.

    Hence, there is no additional GPIO port available in the SMJ320C6701 device.

    Thanks & regards,

    Sivaraj K

    ---------------------------------------------------------------------------------
    Please click the
    Verify Answer button on this post if it answers your question.
    ---------------------------------------------------------------------------------