Other Parts Discussed in Thread: AM3874
Hi,
My customer has a strange issue.
They are using AM3874 and OS is windows Compact7.
WEC7 is booting some kinds of driver software when OS booting.
But now they have an issue with USB driver woriking.
Failure symptom:
* Some error happens, but OS is still working.
* OS haa hang up, and system can't operate
* Screen was black out.
Failure status○
* If USB K/B is not connected to the system's USB port, its system has some failure after half hour working.
* If USB K/B is connected to the system when booting, the system never happened the failures.
* If USB K/B is connected tto the system until K/B LED is turned on, and after that its K/B is disconnected to
the system. In this case, the system never happened the failures.
* If USB K/B is connecting to the system, the system never happened the failure.
I think this symptom shows USB module has some issue. How do you think this case?
Also our customer's WEC7 system has other issue. Please see the below E2E page.
http://e2e.ti.com/support/embedded/wince/f/353/p/258226/905743.aspx#905743
This issue also has not been solved.
I appreciate your quick reply.
Best regards,
Michi