Hi,
Some help here would be appreciated please.
When I output OSD graphics to LCD on fb0 it displays fine. But when I output video to LCD I just get white screen.
Even gstreamer test pipeline is not working well. After retries of the same command pipeline I sometimes get the test video ok.
I also tried the demo App in /ti-dvsdk_dm368-evm_4_02_00_06/dmai_2_20_00_15/packages/ti/sdo/dmai/apps/video_display/linux/video_display_dm368.x470MV
This video test app did not result in any error but it does not display.
Display output: LCD; Mode: Auto
root@dm368-evm:~/dm368# ./video_display_dm368.x470MV -y16 -Olcd -n1000 [NO DISPLAY]
root@dm368-evm:~/dm368#
root@dm368-evm:~/dm368#
root@dm368-evm:~/dm368# ./video_display_dm368.x470MV -y5 -Ocomponent -n1000 [DISPLAY OK]
Display size 1280x720 pitch 1280 x = 0 color 0
Display size 1280x720 pitch 1280 x = 1 color 1
Display size 1280x720 pitch 1280 x = 2 color 2
Regards
Raminder