This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 run 1080P

hi  i wana use DM365  300MHZ  to  run  1080p/20

but the video input from sensor is  1080/30

 Module   | Avg Time/Frame | Frame-rate | Total time | Total Frames |

CAPTURE | 34.28 | 29.17 | 23688 | 691 |
ENCODE0 | 43.62 | 22.93 | 20065 | 460 |
ENCODE1 | 2.65 | 376.74 | 1221 | 460 |
STREAM | 1.41 | 710.97 | 1294 | 920 |
OSD0 | 0.04 | 23033.33 | 30 | 691 |
OSD1 | 0.05 | 19742.86 | 35 | 691 |
AEWB | 1.95 | 512.21 | 1392 | 713 |

the video output ,  some frame lost. 

my question is :  does  DM365 can  capture 1080P/30 or not ?  and only the encode is 1080P/20 is ok?

in this case ,   did i need to set my sensor output  at 1080p/20? ?

  • I think ARM frequency is limiting factor here.

    You may want to go through this.

    http://www.ti.com/lsds/ti/dsp/video_processors/dm3x/products.page?paramCriteria=no#p2115=1%20ARM9&p2121=Single%20channel;Encode&p2119=&p2094=Video%20and%20Imaging&p2102=&p2120=