This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MII and MDIO signal timing characteristics for AM335x PRU

Other Parts Discussed in Thread: TLK110

Our customer uses AM335x PRU as a EtherCAT slave controller. They want to use the PHY which is not TLK110.

The MII and MDIO signal timing characteristics are specified in the IEEE-802.3 specifications.

IEEE 802.3-2012 Section Two
http://standards.ieee.org/getieee802/download/802.3-2012_section2.pdf
22.3.1 Signals that are synchronous to TX_CLK [Page78]
22.3.2 Signals that are synchronous to RX_CLK [Page78]
22.3.4 MDIO timing relationship to MDC [Page79]

Do the MII and MDIO signal timing characteristics for PRU meet this IEEE-802.3 specification?

Best regards,

Daisuke