While going through the hyperlink document I got struck with some basic doubts. I have listed them below.
1) It is said that the hyperlink side band lines are LVCMOS. Then why every side band lines are paired?
2) The protocol description of the side band signaling seems to be too difficult to understand from the hyperlink document.Any elaborated description available?
3) Regarding the initialization of the hyperlink. There is no guarantee that the two participating devices in hyperlink communication to come up/ come out of reset exactly the same time. This can make the resetting sequence initiated by the sender not seen by the receiver. What if the reset sequence sent by the sender of the station management bus is missed by the receiver. How is the initialization is ensured later then?
4) It is said that the MSB of all station management messages are set to zero. Then why do messages 0b1110, 0b1000 and 0b1001 have their MSBs set to 1? Also kindly explain how this mechanism allows the SM bus to differentiate between the message and reset.
5) I am bit confused with flow control, power management, status and capabilities messages. Is status and capabilities messages grouped to one category?