Other Parts Discussed in Thread: TCA6424
HI,
Can you please point out what is the reason for this warning while booting Panda5AJ.1.5 on OMAP5 evm
Is it a significant warning ?
[ 1.402648] ------------[ cut here ]------------
[ 1.407470] WARNING: at arch/arm/mach-omap2/pm4xxx_5xxx.c:751 omap4_pm_init+0x28c/0x558()
[ 1.415954] Enabled DSS->EMIF Static dependency, needs proper rootcause
[ 1.422821] Modules linked in:
[ 1.426055] Backtrace:
[ 1.428649] [<80012e2c>] (dump_backtrace+0x0/0x110) from [<804a512c>] (dump_stack+0x20/0x24)
[ 1.437408] r6:80658004 r5:00000009 r4:ef043f08 r3:811bad80
[ 1.443298] [<804a510c>] (dump_stack+0x0/0x24) from [<80039d30>] (warn_slowpath_common+0x5c/0x74)
[ 1.452484] [<80039cd4>] (warn_slowpath_common+0x0/0x74) from [<80039e04>] (warn_slowpath_fmt+0x40/0x48)
[ 1.462310] r8:811b562c r7:811b553c r6:811b550c r5:811b559c r4:00000000
[ 1.468994] r3:00000009
[ 1.471862] [<80039dc4>] (warn_slowpath_fmt+0x0/0x48) from [<80658004>] (omap4_pm_init+0x28c/0x558)
[ 1.481231] r3:811f89a4 r2:805ac980
[ 1.484985] [<80657d78>] (omap4_pm_init+0x0/0x558) from [<80655a80>] (omap2_common_pm_subsys_init+0xdc/0x16c)
[ 1.495269] r8:000000b0 r7:811f7780 r6:80692a30 r5:805a78d7 r4:811f7e90
[ 1.502227] [<806559a4>] (omap2_common_pm_subsys_init+0x0/0x16c) from [<800087b0>] (do_one_initcall+0xa4/0x174)
[ 1.512664] r5:80676134 r4:00000004
[ 1.516418] [<8000870c>] (do_one_initcall+0x0/0x174) from [<8064ba8c>] (kernel_init+0x158/0x21c)
[ 1.525543] [<8064b934>] (kernel_init+0x0/0x21c) from [<8003e088>] (do_exit+0x0/0x7bc)
[ 1.533752] ---[ end trace ac6d8289a4a03a7a ]---
[ 1.538757] ------------[ cut here ]------------
[ 1.543579] WARNING: at arch/arm/mach-omap2/pm4xxx_5xxx.c:1238 omap4_pm_init+0x484/0x558()
[ 1.552154] omap4_pm_init: EMIF Clock domain denied idle: DDR3 WA
[ 1.558502] Modules linked in:
[ 1.561706] Backtrace:
[ 1.564300] [<80012e2c>] (dump_backtrace+0x0/0x110) from [<804a512c>] (dump_stack+0x20/0x24)
[ 1.573059] r6:806581fc r5:00000009 r4:ef043f08 r3:811bad80
[ 1.578948] [<804a510c>] (dump_stack+0x0/0x24) from [<80039d30>] (warn_slowpath_common+0x5c/0x74)
[ 1.588165] [<80039cd4>] (warn_slowpath_common+0x0/0x74) from [<80039e04>] (warn_slowpath_fmt+0x40/0x48)
[ 1.597961] r8:811b562c r7:811b553c r6:811b550c r5:00000003 r4:00000000
[ 1.604675] r3:00000009
[ 1.607543] [<80039dc4>] (warn_slowpath_fmt+0x0/0x48) from [<806581fc>] (omap4_pm_init+0x484/0x558)
[ 1.616912] r3:804b15ea r2:805acb0d
[ 1.620666] [<80657d78>] (omap4_pm_init+0x0/0x558) from [<80655a80>] (omap2_common_pm_subsys_init+0xdc/0x16c)
[ 1.630950] r8:000000b0 r7:811f7780 r6:80692a30 r5:805a78d7 r4:811f7e90
[ 1.637908] [<806559a4>] (omap2_common_pm_subsys_init+0x0/0x16c) from [<800087b0>] (do_one_initcall+0xa4/0x174)
[ 1.648345] r5:80676134 r4:00000004
[ 1.652099] [<8000870c>] (do_one_initcall+0x0/0x174) from [<8064ba8c>] (kernel_init+0x158/0x21c)
[ 1.661224] [<8064b934>] (kernel_init+0x0/0x21c) from [<8003e088>] (do_exit+0x0/0x7bc)
[ 1.669433] ---[ end trace ac6d8289a4a03a7b ]---
Regards,
Ishaqe