This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

why? omap5432-evm



 

What the hell is going on?
I will trouble?

 

ubuntu $ dmesg

  • Hi,

    Which kernel version are you using?

    I am using GLSDK 6_00_00_07 (http://downloads.ti.com/dsps/dsps_public_sw/glsdk/6_00_00_07/index_FDS.html), which is 3.8.4-100-omap5 GNU/Linux kernel version, and Ubuntu 12.04.

    When I run dmesg  I do not see any of the messages from your post.

    Try updating your linux/android.

    Best Regards,

    Yordan

  • You should use the same version. In the beginning was well.

    But after connecting the monitor to stop WebCamemra, keyboard, and mouse stopping Symptoms appeared in the same post.
    I can not access to the EVM.